powered by CADENAS

Social Share

High-speed steel (6414 views - Material Database)

High-speed steel (HSS or HS) is a subset of tool steels, commonly used as Cutting tool material. It is often used in power-saw blades and drill bits. It is superior to the older high-carbon steel tools used extensively through the 1940s in that it can withstand higher temperatures without losing its temper (hardness). This property allows HSS to cut faster than high carbon steel, hence the name high-speed steel. At room temperature, in their generally recommended heat treatment, HSS grades generally display high hardness (above Rockwell hardness 60) and abrasion resistance (generally linked to tungsten and vanadium content often used in HSS) compared with common carbon and tool steels.
Go to Article

High-speed steel

High-speed steel

High-speed steel

Licensed under Creative Commons Attribution 2.5 se (Riksantikvarieämbetet / Pål-Nils Nilsson, CC-BY).

High-speed steel (HSS or HS) is a subset of tool steels, commonly used as Cutting tool material.

It is often used in power-saw blades and drill bits. It is superior to the older high-carbon steel tools used extensively through the 1940s in that it can withstand higher temperatures without losing its temper (hardness). This property allows HSS to cut faster than high carbon steel, hence the name high-speed steel. At room temperature, in their generally recommended heat treatment, HSS grades generally display high hardness (above Rockwell hardness 60) and abrasion resistance (generally linked to tungsten and vanadium content often used in HSS) compared with common carbon and tool steels.

History

Although development of modern high speed steel began in the second half of the 19th century, there is documented evidence of steels produced earlier with similar content. These include hardened steels in China in 13th century BC, wootz steel manufactured in India around 350 BC and production of Damascus and Japanese layered steel blades in years 540 AD and 900 AD.[1] High-speed properties of those steels would be mostly coincidental (as no machining technology that involved quantification of speeds and feeds existed at the time) and would be the result of local iron ores containing natural traces of tungsten or other favorable alloying components.

In 1868 the English metallurgist Robert Forester Mushet developed Mushet steel, considered to be the forerunner of modern high speed steels. It consisted of 2% carbon (C), 2.5% manganese (Mn), and 7% tungsten (W). The major advantage of this steel was that it hardened when air cooled from a temperature at which most steels had to be quenched for hardening. Over the next 30 years the most significant change was the replacement of manganese (Mn) with chromium (Cr).[2]

In 1899 and 1900, Frederick Winslow Taylor and Maunsel White, working with a team of assistants at the Bethlehem Steel Company at Bethlehem, Pennsylvania, US, performed a series of experiments with the heat treating of existing high-quality tool steels, such as Mushet steel, heating them to much higher temperatures than were typically considered desirable in the industry.[3][4] Their experiments were characterised by a scientific empiricism in that many different combinations were made and tested, with no regard for conventional wisdom or alchemic recipes, and with detailed records kept of each batch. The end result was a heat treatment process that transformed existing alloys into a new kind of steel that could retain its hardness at higher temperatures, allowing much higher speeds and rate of cutting when machining.

The Taylor-White process[5] was patented and created a revolution in the machining industries. Heavier machine tools with higher rigidity were needed to use the new steel to its full advantage, prompting redesigns and replacement of installed plant. The patent was hotly contested and eventually nullified.[6]

The first alloy that was formally classified as high-speed steel is known by the AISI designation T1, which was introduced in 1910.[1] It was patented by Crucible Steel Co. at the beginning of the 20th century.[2]

Although molybdenum-rich high-speed steels such as AISI M1 have been used since the 1930s, material shortages and high costs caused by World War II spurred development of less expensive alloys substituting molybdenum for tungsten. The advances in molybdenum-based high speed steel during this period put them on par with and in certain cases better than tungsten-based high speed steels. This started with the use of M2 steel instead of T1 steel.[2][7]

Types

High speed steels are alloys that gain their properties from either tungsten or molybdenum, often with a combination of the two. They belong to the Fe–C–X multi-component alloy system where X represents chromium, tungsten, molybdenum, vanadium, or cobalt. Generally, the X component is present in excess of 7%, along with more than 0.60% carbon. The alloying element percentages do not alone bestow the hardness-retaining properties; they also require appropriate high-temperature heat treatment to become true HSS; see History above.

In the unified numbering system (UNS), tungsten-type grades (e.g. T1, T15) are assigned numbers in the T120xx series, while molybdenum (e.g. M2, M48) and intermediate types are T113xx. ASTM standards recognize 7 tungsten types and 17 molybdenum types.[8]

The addition of about 10% of tungsten and molybdenum in total maximises efficiently the hardness and toughness of high speed steels and maintains those properties at the high temperatures generated when cutting metals.

A sample of alloying compositions of common high speed steel grades (by %wt)[9][10] (impurity limits are not included)
Grade C Cr Mo W V Co Mn Si
T1 0.65–0.80 4.00 - 18 1 - 0.1–0.4 0.2–0.4
M1 0.80 4 8 1.5 1.0 - - -
M2 0.95 4 5 6.0 2.0 - - -
M7 1.00 4 8.75 1.75 2.0 - - -
M35 0.92 4.3 5 6.4 1.8 5 - 0.35
M42 1.10 3.75 9.5 1.5 1.15 8.0 - -
M50 0.85 4 4.25 .10 1.0 - - -

Tungsten Steels

T1
The original HSS, it has been generally superseded by M2.

Molybdenum High Speed Steels (HSS)

Adding molybdenum, tungsten and chromium steel creates several alloys commonly called "HSS", measuring 63-65 Rockwell hardness.

M1
M1 lacks some of the red-hardness properties of M2, but is less susceptible to shock and will flex more.
M2
M2 is the "standard" and most widely used industrial HSS. It has small and evenly distributed carbides giving high wear resistance, though its decarburization sensitivity is a little bit high. After heat treatment, its hardness is the same as T1, but its bending strength can reach 4700 MPa, and its toughness and thermo-plasticity are higher than T1 by 50%. It is usually used to manufacture a variety of tools, such as drill bits, taps and reamers.
M7
M7 is used for making heavier construction drills where flexibility and extended drill life are equally important.
M50
M50 does not have the red-hardness of other grades of tungsten HSS, but is very good for drills where breakage is a problem due to flexing the drill. Generally favored for hardware stores and contractor use. It is also used in high-temperature ball bearings.

Cobalt High Speed Steels (HSS)

The addition of cobalt increases heat resistance, and can give a Rockwell hardness up to 67 Min..

M35
M35 is similar to M2, but with 5% cobalt added. M35 is also known as Cobalt Steel, HSSE or HSS-E. It will cut faster and last longer than M2.
M42
M42 is a molybdenum-series high-speed steel alloy with an additional 8% or 10% cobalt. It is widely used in metal manufacturing industries because of its superior red-hardness as compared to more conventional high-speed steels, allowing for shorter cycle times in production environments due to higher cutting speeds or from the increase in time between tool changes. M42 is also less prone to chipping when used for interrupted cuts and costs less when compared to the same tool made of carbide. Tools made from cobalt-bearing high speed steels can often be identified by the letters HSS-Co.

Coatings

The life of high-speed steel can be prolonged by coating the tool . One such coating is TiN (titanium nitride). Most coatings generally increase a tool's hardness and/or lubricity. A coating allows the cutting edge of a tool to cleanly pass through the material without having the material gall (stick) to it. The coating also helps to decrease the temperature associated with the cutting process and increase the life of the tool.

Surface modification

Lasers and electron beams can be used as sources of intense heat at the surface for heat treatment, remelting (glazing), and compositional modification. It is possible to achieve different molten pool shapes and temperatures. Cooling rates range from 103 to 106 K s−1. Beneficially, there is little or no cracking or porosity formation.[2]

While the possibilities of heat treating at the surface should be readily apparent, the other applications beg some explanation. At cooling rates in excess of 106 K s−1 eutectic microconstituents disappear and there is extreme segregation of substitutional alloying elements. This has the effect of providing the benefits of a glazed part without the associated run in wear damage.[2]

The alloy composition of a part or tool can also be changed to form a high speed steel on the surface of a lean alloy or to form an alloy or carbide enriched layer on the surface of a high speed steel part. Several methods can be used such as foils, pack boronising, plasma spray powders, powder cored strips, inert gas blow feeders, etc. Although this method has been reported to be both beneficial and stable, it has yet to see widespread commercial use.[2]

Applications

The main use of high-speed steels continues to be in the manufacture of various cutting tools: drills, taps, milling cutters, tool bits, gear cutters, saw blades, planer and jointer blades, router bits, etc., although usage for punches and dies is increasing.

High speed steels also found a market in fine hand tools where their relatively good toughness at high hardness, coupled with high abrasion resistance, made them suitable for low speed applications requiring a durable keen (sharp) edge, such as files, chisels, hand plane blades, and damascus kitchen knives and pocket knives.

High speed steel tools are the most popular for use in woodturning, as the speed of movement of the work past the edge is relatively high for handheld tools, and HSS holds its edge far longer than high carbon steel tools can.

See also


41xx steelAlGaAlnicoAluminiumAluminium alloyAluminium bronzeAluminium-lithium alloyArsenical bronzeArsenical copperBell metalBerylliumBeryllium copperBillon (alloy)BirmabrightBismanolBismuthBrassBronzeBulat steelCalamine brassCast ironChinese silverChromiumChromium hydrideCobaltColored goldConstantanCopperCopper hydrideCopper–tungstenCorinthian bronzeCrown goldCrucible steelCunifeCupronickelCymbal alloysDamascus steelDevarda's alloyDuraluminDutch metalElectrumElinvarFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolGalinstanGalliumGilding metalGlassGlucydurGoldGuanín (bronze)GunmetalHepatizonHiduminiumHydronaliumIndiumInvarIronIron–hydrogen alloyItalmaKanthal (alloy)KovarLeadMagnaliumMagnesiumMangalloyManganinMegalliumMelchior (alloy)MercuryMolybdochalkosMuntz metalNichromeNickelNickel silverNordic GoldOrmoluPhosphor bronzePig ironPinchbeck (alloy)PlasticPlexiglasPlutoniumPotassiumRhoditeRhodiumRose's metalSamariumScandiumShakudōSilverSodiumSpeculum metalSpiegeleisenStaballoyStainless steelSteelStelliteStructural steelTinTitaniumTombacTumbagaUraniumVitalliumWood's metalY alloyZincZirconiumMushet steelMaraging steelHigh-strength low-alloy steelReynolds 531Electrical steelSpring steelAL-6XNCelestriumAlloy 20Marine grade stainlessMartensitic stainless steelSanicro 28Surgical stainless steelZeron 100Silver steelTool steelWeathering steelWootz steelSolderTerneType metalElektron (alloy)Amalgam (chemistry)Magnox (alloy)AlumelBrightrayChromelHaynes InternationalInconelMonelNicrosilNisilNickel titaniumMu-metalPermalloySupermalloyNickel hydridePlutonium–gallium alloySodium-potassium alloyMischmetalLithiumTerfenol-DPseudo palladiumScandium hydrideSamarium–cobalt magnetArgentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichiSterling silverTibetan silverTitanium Beta CTitanium alloyTitanium hydrideGum metalTitanium goldTitanium nitrideBabbitt (alloy)Britannia metalPewterQueen's metalWhite metalUranium hydrideZamakZirconium hydrideHydrogenHeliumBoronNitrogenOxygenFluorineMethaneMezzanineAtomSteel millSteelmaking

This article uses material from the Wikipedia article "High-speed steel", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material