This article does not cite any sources. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (December 2009) (Learn how and when to remove this template message) |
Elinvar is a nickel-iron alloy notable for having a modulus of elasticity which does not change much with temperature changes. The name is a contraction of the French elasticité invariable (elastically invariable). It was invented by Charles Édouard Guillaume, a Swiss physicist who also invented Invar, another alloy of nickel and iron with very low thermal expansion. Guillaume won the 1920 Nobel Prize in Physics for these discoveries, which shows how important these alloys were for scientific instruments.
Elinvar consists of 59% iron, 36% nickel, and 5% chromium. It is almost nonmagnetic and corrosion resistant.
Other variations of elinvar alloy are
The largest use of Elinvar was in balance springs for mechanical watches and chronometers. A major cause of inaccuracy in watches and clocks was that ordinary steels used in springs lost elasticity slightly as the temperature increased, so the balance wheel would oscillate more slowly back and forth, and the clock would lose time. Chronometers and precision watches required complex temperature-compensated balance wheels for accurate timekeeping. Springs made of Elinvar, and other low temperature coefficient alloys such as Nivarox that followed, were not affected by temperature, so they made the temperature-compensated balance wheel obsolete.
This alloy-related article is a stub. You can help Wikipedia by expanding it. |
This article uses material from the Wikipedia article "Elinvar", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
database,rohs,reach,compliancy,directory,listing,information,substance,material