Megallium is a trademark for an alloy of 60% cobalt, 20% chromium, 5% molybdenum, and traces of other substances. The alloy is used in dentistry because of its light weight, resistance to corrosion and hypo-allergenic (nickel free) properties. Megallium was developed by John Leonard Attenborough for Attenborough Dental Laboratories in 1951.
This alloy-related article is a stub. You can help Wikipedia by expanding it. |
This article uses material from the Wikipedia article "Megallium", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
database,rohs,reach,compliancy,directory,listing,information,substance,material