powered by CADENAS

Social Share

Plastic (9995 views - Material Database)

Plastic is material consisting of any of a wide range of synthetic or semi-synthetic organic compounds that are malleable and so can be molded into solid objects. Plasticity is the general property of all materials which can deform irreversibly without breaking but, in the class of moldable polymers, this occurs to such a degree that their actual name derives from this ability. Plastics are typically organic polymers of high molecular mass, but they often contain other substances. They are usually synthetic, most commonly derived from petrochemicals, but many are made from renewable materials such as polylactic acid from corn or cellulosics from cotton linters. Due to their relatively low cost, ease of manufacture, versatility, and imperviousness to water, plastics are used in an enormous and expanding range of products, from paper clips to spaceships. They have already displaced many traditional materials, such as wood, stone, horn and bone, leather, paper, metal, glass, and ceramic, in most of their former uses. In developed countries, about a third of plastic is used in packaging and another third in buildings such as piping used in plumbing or vinyl siding. Other uses include automobiles (up to 20% plastic), furniture, and toys. In the developing world, the ratios may be different - for example, reportedly 42% of India's consumption is used in packaging. Plastics have many uses in the medical field as well, to include polymer implants, however the field of plastic surgery is not named for use of plastic materials, but rather the more generic meaning of the word plasticity, with regard to the reshaping of flesh. The world's first fully synthetic plastic was bakelite, invented in New York in 1907 by Leo Baekeland who coined the term 'plastics'. Many chemists have contributed to the materials science of plastics, including Nobel laureate Hermann Staudinger who has been called "the father of polymer chemistry" and Herman Mark, known as "the father of polymer physics". The success and dominance of plastics starting in the early 20th century led to environmental concerns regarding its slow decomposition rate after being discarded as trash due to its composition of very large molecules. Toward the end of the century, one approach to this problem was met with wide efforts toward recycling.
Go to Article

Explanation by Hotspot Model

Plastic

Plastic

IUPAC definition
Generic term used in the case of polymeric material that may contain other substances to improve performance and/or reduce costs.

Note 1: The use of this term instead of polymer is a source of confusion and thus is not recommended.

Note 2: This term is used in polymer engineering for materials often compounded that can be processed by flow.[1]

Plastic is material consisting of any of a wide range of synthetic or semi-synthetic organic compounds that are malleable and so can be molded into solid objects.

Plasticity is the general property of all materials which can deform irreversibly without breaking but, in the class of moldable polymers, this occurs to such a degree that their actual name derives from this ability.

Plastics are typically organic polymers of high molecular mass, but they often contain other substances. They are usually synthetic, most commonly derived from petrochemicals, but many are made from renewable materials such as polylactic acid from corn or cellulosics from cotton linters.[2]

Due to their relatively low cost, ease of manufacture, versatility, and imperviousness to water, plastics are used in an enormous and expanding range of products, from paper clips to spaceships. They have already displaced many traditional materials, such as wood, stone, horn and bone, leather, paper, metal, glass, and ceramic, in most of their former uses.

In developed countries, about a third of plastic is used in packaging and another third in buildings such as piping used in plumbing or vinyl siding.[3] Other uses include automobiles (up to 20% plastic[3]), furniture, and toys.[3] In the developing world, the ratios may be different - for example, reportedly 42% of India's consumption is used in packaging.[3]

Plastics have many uses in the medical field as well, to include polymer implants, however the field of plastic surgery is not named for use of plastic materials, but rather the more generic meaning of the word plasticity, with regard to the reshaping of flesh.

The world's first fully synthetic plastic was bakelite, invented in New York in 1907 by Leo Baekeland[4] who coined the term 'plastics'.[5] Many chemists have contributed to the materials science of plastics, including Nobel laureate Hermann Staudinger who has been called "the father of polymer chemistry" and Herman Mark, known as "the father of polymer physics".[6]

The success and dominance of plastics starting in the early 20th century led to environmental concerns regarding its slow decomposition rate after being discarded as trash due to its composition of very large molecules. Toward the end of the century, one approach to this problem was met with wide efforts toward recycling.

Etymology

The word plastic derives from the Greek πλαστικός (plastikos) meaning "capable of being shaped or molded" and, in turn, from πλαστός (plastos) meaning "molded".[7][8]

The plasticity, or malleability, of the material during manufacture allows it to be cast, pressed, or extruded into a variety of shapes, such as: films, fibers, plates, tubes, bottles, boxes, amongst many others.

The common noun plastic should not be confused with the technical adjective plastic. The adjective is applicable to any material which undergoes a plastic deformation, or permanent change of shape, when strained beyond a certain point. For example, aluminum which is stamped or forged exhibits plasticity in this sense, but is not plastic in the common sense. By contrast, some plastics will, in their finished forms, break before deforming and therefore are not plastic in the technical sense.

Structure

Most plastics contain organic polymers.[9] The vast majority of these polymers are formed from chains of carbon atoms, 'pure' or with the addition of: oxygen, nitrogen, or sulfur. The chains comprise many repeat units, formed from monomers. Each polymer chain will have several thousand repeating units.

The backbone is the part of the chain that is on the "main path", linking together a large number of repeat units.

To customize the properties of a plastic, different molecular groups "hang" from this backbone. In reality, however, the "pendant units" are usually "hung" as part of the monomers, before the monomers themselves are linked together to form the polymer chain. It is the structure of these side chains that influences the properties of the polymer.

The molecular structure of the repeating unit can be fine tuned to influence specific properties in the polymer.

Properties and Classifications

Plastics are usually classified by: the chemical structure of the polymer's backbone and side chains; some important groups in these classifications are: the acrylics, polyesters, silicones, polyurethanes, and halogenated plastics.

Plastics can also be classified by: the chemical process used in their synthesis, such as: condensation, polyaddition, and cross-linking.[10]

Plastics can also be classified by: their various physical properties, such as: hardness, density, tensile strength, resistance to heat and glass transition temperature, and by their chemical properties, such as the organic chemistry of the polymer and its resistance and reaction to various chemical products and processes, such as: organic solvents, oxidation, and ionizing radiation. In particular, most plastics will melt upon heating to a few hundred degrees celsius.[11]

Other classifications are based on qualities that are relevant for manufacturing or product design. Examples of such qualities and classes are: thermoplastics and thermosets, conductive polymers, biodegradable plastics and engineering plastics and other plastics with particular structures, such as elastomers.

Thermoplastics and thermosetting polymers

One important classification of plastics is by the permanence or impermanence of their form, or whether they are: thermoplastics or thermosetting polymers. Thermoplastics are the plastics that, when heated, do not undergo chemical change in their composition and so can be molded again and again. Examples include: polyethylene (PE), polypropylene (PP), polystyrene (PS) and polyvinyl chloride (PVC).[12] Common thermoplastics range from 20,000 to 500,000 amu, while thermosets are assumed to have infinite molecular weight.

Thermosets, or thermosetting polymers, can melt and take shape only once: after they have solidified, they stay solid.[13] In the thermosetting process, a chemical reaction occurs that is irreversible. The vulcanization of rubber is an example of a thermosetting process: before heating with sulfur, the polyisoprene is a tacky, slightly runny material; after vulcanization, the product is rigid and non-tacky.

Amorphous plastics and crystalline plastics

Many plastics are completely amorphous,[14] such as: all thermosets; polystyrene and its copolymers; and polymethyl methacrylate.

However, some plastics are partially crystalline and partially amorphous in molecular structure, giving them both a melting point, the temperature at which the attractive intermolecular forces are overcome, and also one or more glass transitions, the temperatures above which the extent of localized molecular flexibility is substantially increased. These so-called semi-crystalline plastics include: polyethylene, polypropylene, polyvinyl chloride, polyamides (nylons), polyesters and some polyurethanes.

Conductive Polymers

Intrinsically Conducting Polymers (ICP) are organic polymers that conduct electricity. While plastics can be made electrically conductive, with a conductivity of up to 80 kS/cm in stretch-oriented polyacetylene,[15] they are still no match for most metals like copper which have a conductivity of several hundred kS/cm. Nevertheless, this is a developing field.

Biodegradable plastics and bioplastics

Biodegradable plastics are plastics that degrade, or break down, upon exposure to: sunlight or ultra-violet radiation, water or dampness, bacteria, enzymes or wind abrasion. In some instances, rodent, pest, or insect attack can also be considered as forms of biodegradation or environmental degradation.

Some modes of degradation require that the plastic be exposed at the surface (aerobic), whereas other modes will only be effective if certain conditions exist in landfill or composting systems (anaerobic).

Some companies produce biodegradable additives, to enhance biodegradation. Plastic can have starch powder added as a filler to allow it to degrade more easily, but this still does not lead to the complete breaking down of the plastic.

Some researchers have genetically engineered bacteria to synthesize completely biodegradable plastics, such as Biopol; however, these are expensive at present.[16]

Bioplastics

Whilst most plastics are produced from petrochemicals, bioplastics are made substantially from renewable plant materials such: as cellulose and starch.[17] Due both to the finite limits of the petrochemical reserves and to the threat of global warming, the development of bioplastics is a growing field.

However, bioplastic development begins from a very low base and, as yet, does not compare significantly with petrochemical production. Estimates of the global production capacity for bio-derived materials is put at 327,000 tonnes/year, out of a global consumption, of all flexible packaging, estimated at 12.3 million tonnes/year.[18][19]

Types

Common plastics

This category includes both commodity plastics, or standard plastics, and engineering plastics.

  • Polyamides (PA) or (nylons) – fibers, toothbrush bristles, tubing, fishing line and low-strength machine parts such as engine parts or gun frames
  • Polycarbonate (PC) – compact discs, eyeglasses, riot shields, security windows, traffic lights and lenses
  • Polyester (PES) – fibers and textiles
  • Polyethylene (PE) – a wide range of inexpensive uses including supermarket bags and plastic bottles
  • Polypropylene (PP) – bottle caps, drinking straws, yogurt containers, appliances, car fenders (bumpers) and plastic pressure pipe systems
  • Polystyrene (PS) – foam peanuts, food containers, plastic tableware, disposable cups, plates, cutlery, compact-disc (CD) and cassette boxes
  • Polyurethanes (PU) – cushioning foams, thermal insulation foams, surface coatings and printing rollers: currently the sixth or seventh most commonly-used plastic, for instance the most commonly used plastic in cars
  • Polyvinyl chloride (PVC) – plumbing pipes and guttering, shower curtains, window frames and flooring
  • Polyvinylidene chloride (PVDC) – food packaging, such as: Saran
  • Acrylonitrile butadiene styrene (ABS) – electronic equipment cases (e.g. computer monitors, printers, keyboards) and drainage pipe
    • Polycarbonate/Acrylonitrile Butadiene Styrene (PC/ABS) – a blend of PC and ABS that creates a stronger plastic used in car interior and exterior parts, and mobile phone bodies
    • Polyethylene/Acrylonitrile Butadiene Styrene (PE/ABS) – a slippery blend of PE and ABS used in low-duty dry bearings

Specialist plastics

  • Polyepoxide (epoxy) – used as an adhesive, potting agent for electrical components, and matrix for composite materials with hardeners including amine, amide, and boron trifluoride
  • Polymethyl methacrylate (PMMA) (acrylic) – contact lenses (of the original "hard" variety), glazing (best known in this form by its various trade names around the world; e.g. Perspex, Plexiglas, Oroglas), aglets, fluorescent light diffusers, rear light covers for vehicles. It forms the basis of artistic and commercial acrylic paints when suspended in water with the use of other agents.
  • Polytetrafluoroethylene (PTFE), or Teflon – heat-resistant, low-friction coatings, used in things like non-stick surfaces for frying pans, plumber's tape and water slides
  • Phenolics or phenol formaldehyde (PF) – high modulus, relatively heat resistant, and excellent fire resistant polymer. Used for insulating parts in electrical fixtures, paper laminated products (e.g. Formica), thermally insulation foams. It is a thermosetting plastic, with the familiar trade name Bakelite, that can be molded by heat and pressure when mixed with a filler-like wood flour or can be cast in its unfilled liquid form or cast as foam (e.g. Oasis). Problems include the probability of moldings naturally being dark colors (red, green, brown), and as thermoset it is difficult to recycle.
  • Melamine formaldehyde (MF) – one of the aminoplasts, used as a multi-colorable alternative to phenolics, for instance in moldings (e.g. break-resistance alternatives to ceramic cups, plates and bowls for children) and the decorated top surface layer of the paper laminates (e.g. Formica)
  • Urea-formaldehyde (UF) – one of the aminoplasts, used as a multi-colorable alternative to phenolics: used as a wood adhesive (for plywood, chipboard, hardboard) and electrical switch housings.
  • Polyetheretherketone (PEEK) – strong, chemical- and heat-resistant thermoplastic, biocompatibility allows for use in medical implant applications, aerospace moldings. One of the most expensive commercial polymers.
  • Maleimide/bismaleimide – used in high temperature composite materials
  • Polyetherimide (PEI) (Ultem) – a high temperature, chemically stable polymer that does not crystallize
  • Polyimide – a high temperature plastic used in materials such as Kapton tape
  • Plastarch material – biodegradable and heat-resistant thermoplastic composed of modified corn starch
  • Polylactic acid (PLA) – a biodegradable, thermoplastic found converted into a variety of aliphatic polyesters derived from lactic acid, which in turn can be made by fermentation of various agricultural products such as cornstarch, once made from dairy products
  • Furan – resin based on furfuryl alcohol used in foundry sands and biologically derived composites
  • Silicone – heat resistant resin used mainly as a sealant but also used for high temperature cooking utensils and as a base resin for industrial paints
  • Polysulfone – high temperature melt processable resin used in membranes, filtration media, water heater dip tubes and other high temperature applications

History

The development of plastics has evolved from the use of natural plastic materials (e.g., chewing gum, shellac) to the use of chemically modified, natural materials (e.g., natural rubber, nitrocellulose, collagen, galalite) and finally to completely synthetic molecules (e.g., bakelite, epoxy, polyvinyl chloride). Early plastics were bio-derived materials such as egg and blood proteins, which are organic polymers. In 1600 BC, Mesoamericans used natural rubber for balls, bands, and figurines.[3] Treated cattle horns were used as windows for lanterns in the Middle Ages. Materials that mimicked the properties of horns were developed by treating milk-proteins (casein) with lye.

In the 1800s, as industrial chemistry developed during the Industrial Revolution, many materials were reported. The development of plastics also accelerated with Charles Goodyear's discovery of vulcanization to thermoset materials derived from natural rubber.

Parkesine (nitrocellulose) is considered the first man-made plastic. The plastic material was patented by Alexander Parkes, In Birmingham, UK in 1856.[20] It was unveiled at the 1862 Great International Exhibition in London.[21] Parkesine won a bronze medal at the 1862 World's fair in London. Parkesine was made from cellulose (the major component of plant cell walls) treated with nitric acid as a solvent. The output of the process (commonly known as cellulose nitrate or pyroxilin) could be dissolved in alcohol and hardened into a transparent and elastic material that could be molded when heated.[22] By incorporating pigments into the product, it could be made to resemble ivory.

In 1897, the Hanover, Germany mass printing press owner Wilhelm Krische was commissioned to develop an alternative to blackboards.[23] The resultant horn-like plastic made from the milk protein casein was developed in cooperation with the Austrian chemist (Friedrich) Adolph Spitteler (1846–1940). The final result was unsuitable for the original purpose.[24] In 1893, French chemist Auguste Trillat discovered the means to insolubilize casein by immersion in formaldehyde, producing material marketed as galalith.[23]

In the early 1900s, Bakelite, the first fully synthetic thermoset, was reported by Belgian chemist Leo Baekeland by using phenol and formaldehyde.

After World War I, improvements in chemical technology led to an explosion in new forms of plastics, with mass production beginning in the 1940s and 1950s (around World War II).[25] Among the earliest examples in the wave of new polymers were polystyrene (PS), first produced by BASF in the 1930s,[3] and polyvinyl chloride (PVC), first created in 1872 but commercially produced in the late 1920s.[3] In 1923, Durite Plastics Inc. was the first manufacturer of phenol-furfural resins.[26] In 1933, polyethylene was discovered by Imperial Chemical Industries (ICI) researchers Reginald Gibson and Eric Fawcett.[3]

In 1954, polypropylene was discovered by Giulio Natta and began to be manufactured in 1957.[3]

In 1954, expanded polystyrene (used for building insulation, packaging, and cups) was invented by Dow Chemical.[3] Polyethylene terephthalate (PET)'s discovery is credited to employees of the Calico Printers' Association in the UK in 1941; it was licensed to DuPont for the USA and ICI otherwise, and as one of the few plastics appropriate as a replacement for glass in many circumstances, resulting in widespread use for bottles in Europe.[3]

Plastics Industry

Plastics manufacturing is a major part of the chemical industry, and some of the world's largest chemical companies have been involved since the earliest days, such as the industry leaders BASF and Dow Chemical.

In 2014, sales of the top fifty companies amounted to US$961,300,000,000.[27] The firms came from some eighteen countries in total, with more than half of the companies on the list being headquartered in the US. Many of the top fifty plastics companies were concentrated in just three countries:

BASF was the world's largest chemical producer for the ninth year in a row.[27]

Trade associations which represent the industry in the US include the American Chemistry Council.

Industry standards

Many of the properties of plastics are determined by standards specified by ISO, such as:

Many of the properties of plastics are determined by the UL Standards, tests specified by Underwriters Laboratories (UL), such as:

Additives

Blended into most plastics are additional organic or inorganic compounds . The average content of additives is a few percent. Many of the controversies associated with plastics actually relate to the additives:[28] organotin compounds are particularly toxic.[29]

Typical additives include:

Stabilizers

Stabilizers prolong the lifetime of the polymer by suppressing degradation that results from UV-light, oxidation, and other phenomena. Typical stabilzers thus absorb UV light or function as antioxidants.

Fillers

Many plastics[citation needed] contain fillers, to improve performance or reduce production costs.[30] Typically fillers are mineral in origin, e.g., chalk. Other fillers include: starch, cellulose, wood flour, ivory dust and zinc oxide.

Plasticizers

Plasticizers are, by mass, often the most abundant additives.[29] These oily but nonvolatile compounds are blended in to plastics to improve rheology, as many organic polymers are otherwise too rigid for particular applications.

Dioctyl phthalate is the most common plasticizer.

Colorants

Colorants are another common additive, though their weight contribution is small.

Toxicity

Pure plastics have low toxicity due to their insolubility in water and because they are biochemically inert, due to a large molecular weight. Plastic products contain a variety of additives, some of which can be toxic. For example, plasticizers like adipates and phthalates are often added to brittle plastics like polyvinyl chloride to make them pliable enough for use in food packaging, toys, and many other items. Traces of these compounds can leach out of the product. Owing to concerns over the effects of such leachates, the European Union has restricted the use of DEHP (di-2-ethylhexyl phthalate) and other phthalates in some applications, and the United States has limited the use of DEHP, DPB, BBP, DINP, DIDP, and DnOP in children's toys and child care articles with the Consumer Product Safety Improvement Act. Some compounds leaching from polystyrene food containers have been proposed to interfere with hormone functions and are suspected human carcinogens.[32] Other chemicals of potential concern include alkylphenols.[29]

Whereas the finished plastic may be non-toxic, the monomers used in the manufacture of the parent polymers may be toxic. In some cases, small amounts of those chemicals can remain trapped in the product unless suitable processing is employed. For example, the World Health Organization's International Agency for Research on Cancer (IARC) has recognized vinyl chloride, the precursor to PVC, as a human carcinogen.[32]

Bisphenol A (BPA)

Some polymers may also decompose into the monomers or other toxic substances when heated. In 2011, it was reported that "almost all plastic products" sampled released chemicals with estrogenic activity, although the researchers identified plastics which did not leach chemicals with estrogenic activity.[33]

The primary building block of polycarbonates, bisphenol A (BPA), is an estrogen-like endocrine disruptor that may leach into food.[32] Research in Environmental Health Perspectives finds that BPA leached from the lining of tin cans, dental sealants and polycarbonate bottles can increase body weight of lab animals' offspring.[34] A more recent animal study suggests that even low-level exposure to BPA results in insulin resistance, which can lead to inflammation and heart disease.[35]

As of January 2010, the LA Times newspaper reports that the United States FDA is spending $30 million to investigate indications of BPA being linked to cancer.[36]

Bis(2-ethylhexyl) adipate, present in plastic wrap based on PVC, is also of concern, as are the volatile organic compounds present in new car smell.

The European Union has a permanent ban on the use of phthalates in toys. In 2009, the United States government banned certain types of phthalates commonly used in plastic.[37]

Environmental effects

Most plastics are durable and degrade very slowly; the very chemical bonds that make them so durable tend to make them resistant to most natural processes of degradation. However, microbial species and communities capable of degrading plastics are discovered from time to time, and some show promise as being useful for bioremediating certain classes of plastic waste.

Since the 1950s, one billion tons of plastic have been discarded and some of that material might persist for centuries or much longer, as is demonstrated by the persistence of natural materials such as amber.[60]

Serious environmental threats from plastic have been suggested in the light of the increasing presence of microplastics in the marine food chain along with many highly toxic chemical pollutants that accumulate in plastics. They also accumulate in larger fragmented pieces of plastic called nurdles.[61] In the 1960s the latter were observed in the guts of seabirds, and since then have been found in increasing concentration.[62] In 2009, it was estimated that 10% of modern waste was plastics,[25] although estimates vary according to region.[62] Meanwhile, 50-80% of debris in marine areas is plastic.[62]

Before the ban on the use of CFCs in extrusion of polystyrene (and in general use, except in life-critical fire suppression systems; see Montreal Protocol), the production of polystyrene contributed to the depletion of the ozone layer, but current extrusion processes use non-CFCs.

Climate change

The effect of plastics on global warming is mixed. Plastics are generally made from petroleum. If the plastic is incinerated, it increases carbon emissions; if it is placed in a landfill, it becomes a carbon sink[63] although biodegradable plastics have caused methane emissions. [64] Due to the lightness of plastic versus glass or metal, plastic may reduce energy consumption. For example, packaging beverages in PET plastic rather than glass or metal is estimated to save 52% in transportation energy.[3]

Production of plastics

Production of plastics from crude oil requires 62 to 108 MJ/Kg (taking into account the average efficiency of US utility stations of 35%). Producing silicon and semiconductors for modern electronic equipment is even more energy consuming: 230 to 235 MJ/Kg of silicon, and about 3,000 MJ/Kg of semiconductors.[65] This is much higher than the energy needed to produce many other materials, e.g. iron (from iron ore) requires 20-25 MJ/Kg of energy, glass (from sand, etc.) 18-35 MJ/Kg, steel (from iron) 20-50 MJ/Kg, paper (from timber) 25-50 MJ/Kg.[66]

Incineration of plastics

Controlled high-temperature incineration, above 850º C for two seconds,[67] performed with selective additional heating, breaks down toxic dioxins and furans from burning plastic, and is widely used in municipal solid waste incineration.[67] Municipal solid waste incinerators also normally include flue gas treatments to reduce pollutants further.[67] This is needed because uncontrolled incineration of plastic produces polychlorinated dibenzo-p-dioxins, a carcinogen (cancer causing chemical). The problem occurs because the heat content of the waste stream varies.[68] Open-air burning of plastic occurs at lower temperatures, and normally releases such toxic fumes.

Pyrolytic disposal

Plastics can be pyrolyzed into hydrocarbon fuels, since plastics include hydrogen and carbon. One kilogram of waste plastic produces roughly a liter of hydrocarbon.[69]

Recycling

Thermoplastics can be remelted and reused, and thermoset plastics can be ground up and used as filler, although the purity of the material tends to degrade with each reuse cycle. There are methods by which plastics can be broken down to a feedstock state.

The greatest challenge to the recycling of plastics is the difficulty of automating the sorting of plastic wastes, making it labor-intensive. Typically, workers sort the plastic by looking at the resin identification code, although common containers like soda bottles can be sorted from memory. Typically, the caps for PETE bottles are made from a different kind of plastic which is not recyclable, which presents additional problems for the sorting process. Other recyclable materials such as metals are easier to process mechanically. However, new processes of mechanical sorting are being developed to increase the capacity and efficiency of plastic recycling.

While containers are usually made from a single type and color of plastic, making them relatively easy to sort, a consumer product like a cellular phone may have many small parts consisting of over a dozen different types and colors of plastics. In such cases, the resources it would take to separate the plastics far exceed their value and the item is discarded. However, developments are taking place in the field of active disassembly, which may result in more product components being reused or recycled. Recycling certain types of plastics can be unprofitable as well. For example, polystyrene is rarely recycled because the process is usually not cost effective. These unrecycled wastes are typically disposed of in landfills, incinerated or used to produce electricity at waste-to-energy plants.

An early success in the recycling of plastics is Vinyloop, an industrial process to separate PVC from other materials through dissolution, filtration and separation of contaminants. A solvent is used in a closed loop to elute PVC from the waste. This makes it possible to recycle composite PVC waste, which is normally incinerated or put in a landfill. Vinyloop-based recycled PVC's primary energy demand is 46 percent lower than conventionally produced PVC. The global warming potential is 39 percent lower. This is why the use of recycled material leads to a significantly better ecological outcome.[70] This process was used after the Olympic Games in London 2012. Parts of temporary Buildings like the Water Polo Arena and the Royal Artillery Barracks were recycled. In this way, the PVC Policy could be fulfilled, which says that no PVC waste should be left after the games had ended.[71]

In 1988, to assist recycling of disposable items, the Plastic Bottle Institute of the U.S. Society of the Plastics Industry devised a now-familiar scheme to mark plastic bottles by plastic type. Under this scheme, a plastic container is marked with a triangle of three "chasing arrows", which encloses a number denoting the plastic type:

  1. Polyethylene terephthalate (PET or PETE)
  2. High-density polyethylene (HDPE)
  3. Polyvinyl chloride (PVC)
  4. Low-density polyethylene (LDPE)
  5. Polypropylene (PP)
  6. Polystyrene (PS)
  7. Other types of plastic (see list below)

Representative polymers

Bakelite

The first plastic based on a synthetic polymer was made from phenol and formaldehyde, with the first viable and cheap synthesis methods invented in 1907, by Leo Hendrik Baekeland, a Belgian-born American living in New York state. Baekeland was looking for an insulating shellac to coat wires in electric motors and generators. He found that combining phenol (C6H5OH) and formaldehyde (HCOH) formed a sticky mass and later found that the material could be mixed with wood flour, asbestos, or slate dust to create strong and fire resistant "composite" materials. The new material tended to foam during synthesis, requiring that Baekeland build pressure vessels to force out the bubbles and provide a smooth, uniform product, as he announced in 1909, in a meeting of the American Chemical Society.[73] Bakelite was originally used for electrical and mechanical parts, coming into widespread use in consumer goods and jewelry in the 1920s. Bakelite was a purely synthetic material, not derived from living matter. It was also an early thermosetting plastic.

Polystyrene

Styrene polymerization

Unplasticised polystyrene is a rigid, brittle, inexpensive plastic that has been used to make plastic model kits and similar knick-knacks. It also is the basis for some of the most popular "foamed" plastics, under the name styrene foam or Styrofoam. Like most other foam plastics, foamed polystyrene can be manufactured in an "open cell" form, in which the foam bubbles are interconnected, as in an absorbent sponge, and "closed cell", in which all the bubbles are distinct, like tiny balloons, as in gas-filled foam insulation and flotation devices. In the late 1950s, high impact styrene was introduced, which was not brittle. It finds much current use as the substance of toy figurines and novelties.

Polyvinyl chloride

Vinylchloride polymerization

Polyvinyl chloride (PVC, commonly called "vinyl")[74] incorporates chlorine atoms. The C-Cl bonds in the backbone are hydrophobic and resist oxidation (and burning). PVC is stiff, strong, heat and weather resistant, properties that recommend its use in devices for plumbing, gutters, house siding, enclosures for computers and other electronics gear. PVC can also be softened with chemical processing, and in this form it is now used for shrink-wrap, food packaging, and rain gear.

All PVC polymers are degraded by heat and light. When this happens, hydrogen chloride is released into the atmosphere and oxidation of the compound occurs.[75] Because hydrogen chloride readily combines with water vapor in the air to form hydrochloric acid,[76] polyvinyl chloride is not recommended for long-term archival storage of silver, photographic film or paper (mylar is preferable).[77]

Nylon

The plastics industry was revolutionized in the 1930s with the announcement of polyamide (PA), far better known by its trade name nylon. Nylon was the first purely synthetic fiber, introduced by DuPont Corporation at the 1939 World's Fair in New York City.

In 1927, DuPont had begun a secret development project designated Fiber66, under the direction of Harvard chemist Wallace Carothers and chemistry department director Elmer Keiser Bolton. Carothers had been hired to perform pure research, and he worked to understand the new materials' molecular structure and physical properties. He took some of the first steps in the molecular design of the materials.

His work led to the discovery of synthetic nylon fiber, which was very strong but also very flexible. The first application was for bristles for toothbrushes. However, Du Pont's real target was silk, particularly silk stockings. Carothers and his team synthesized a number of different polyamides including polyamide 6.6 and 4.6, as well as polyesters.[78]

General condensation polymerization reaction for nylon

It took DuPont twelve years and US$27 million to refine nylon, and to synthesize and develop the industrial processes for bulk manufacture. With such a major investment, it was no surprise that Du Pont spared little expense to promote nylon after its introduction, creating a public sensation, or "nylon mania".

Nylon mania came to an abrupt stop at the end of 1941 when the USA entered World War II. The production capacity that had been built up to produce nylon stockings, or just nylons, for American women was taken over to manufacture vast numbers of parachutes for fliers and paratroopers. After the war ended, DuPont went back to selling nylon to the public, engaging in another promotional campaign in 1946 that resulted in an even bigger craze, triggering the so-called nylon riots.

Subsequently, polyamides 6, 10, 11, and 12 have been developed based on monomers which are ring compounds; e.g. caprolactam. Nylon 66 is a material manufactured by condensation polymerization.

Nylons still remain important plastics, and not just for use in fabrics. In its bulk form it is very wear resistant, particularly if oil-impregnated, and so is used to build gears, plain bearings, valve seats, seals and because of good heat-resistance, increasingly for under-the-hood applications in cars, and other mechanical parts.

Poly(methyl methacrylate)

Poly(methyl methacrylate) (PMMA), also known as acrylic or acrylic glass as well as by the trade names Plexiglas, Acrylite, Lucite, and Perspex among several others (see below), is a transparent thermoplastic often used in sheet form as a lightweight or shatter-resistant alternative to glass. The same material can be utilised as a casting resin, in inks and coatings, and has many other uses.

Rubber

Natural rubber is an elastomer (an elastic hydrocarbon polymer) that originally was derived from latex, a milky colloidal suspension found in specialised vessels in some plants. It is useful directly in this form (indeed, the first appearance of rubber in Europe was cloth waterproofed with unvulcanized latex from Brazil). However, in 1839, Charles Goodyear invented vulcanized rubber; a form of natural rubber heated with sulfur (and a few other chemicals), forming cross-links between polymer chains (vulcanization), improving elasticity and durability.

In 1851, Nelson Goodyear added fillers to natural rubber materials to form ebonite.[31]

Synthetic rubber

The first fully synthetic rubber was synthesized by Sergei Lebedev in 1910. In World War II, supply blockades of natural rubber from South East Asia caused a boom in development of synthetic rubber, notably styrene-butadiene rubber. In 1941, annual production of synthetic rubber in the U.S. was only 231 tonnes which increased to 840,000 tonnes in 1945. In the space race and nuclear arms race, Caltech researchers experimented with using synthetic rubbers for solid fuel for rockets. Ultimately, all large military rockets and missiles would use synthetic rubber based solid fuels, and they would also play a significant part in the civilian space effort.

See also


Coffee cupDisposable cupAluminiumBismuthCobaltCopperArsenical copperGalliumGoldIndiumIronLeadMercuryNickelPlutoniumRhodiumSilverSamariumTinUraniumZincZirconiumAluminium-lithium alloyAlnicoBirmabrightDuraluminHiduminiumHydronaliumItalmaMagnaliumAluminium alloyY alloyWood's metalRose's metalChromium hydrideNichromeMegalliumStelliteVitalliumBeryllium copperBillon (alloy)BrassCalamine brassChinese silverDutch metalGilding metalMuntz metalPinchbeck (alloy)TombacBronzeAluminium bronzeArsenical bronzeBell metalFlorentine bronzeGlucydurGuanín (bronze)GunmetalPhosphor bronzeOrmoluSpeculum metalConstantanCopper hydrideCopper–tungstenCorinthian bronzeCunifeCupronickelCymbal alloysDevarda's alloyElectrumHepatizonManganinMelchior (alloy)Nickel silverMolybdochalkosNordic GoldShakudōTumbagaAlGaGalfenolGalinstanColored goldRhoditeCrown goldElinvarField's metalFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumInvarCast ironIron–hydrogen alloyPig ironKanthal (alloy)KovarStaballoyBulat steelCrucible steel41xx steelDamascus steelMangalloyHigh-speed steelMushet steelMaraging steelHigh-strength low-alloy steelReynolds 531Electrical steelSpring steelAL-6XNCelestriumAlloy 20Marine grade stainlessMartensitic stainless steelSanicro 28Surgical stainless steelZeron 100Silver steelTool steelWeathering steelWootz steelSolderTerneType metalElektron (alloy)Amalgam (chemistry)Magnox (alloy)AlumelBrightrayChromelHaynes InternationalInconelMonelNicrosilNisilNickel titaniumMu-metalPermalloySupermalloyNickel hydridePlutonium–gallium alloySodium-potassium alloyMischmetalLithiumTerfenol-DPseudo palladiumScandium hydrideSamarium–cobalt magnetArgentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichiSterling silverTibetan silverTitanium Beta CTitanium alloyTitanium hydrideGum metalTitanium goldTitanium nitrideBabbitt (alloy)Britannia metalPewterQueen's metalWhite metalUranium hydrideZamakZirconium hydrideHydrogenHeliumBoronNitrogenOxygenFluorineMethaneMezzanineComposite materialAtomCeramicPlastic pollutionSight glassInjection molding machineStretch wrap

This article uses material from the Wikipedia article "Plastic", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material