powered by CADENAS

Social Share

Slavonski Brod (4292 views - 3D Maps & GIS)

Slavonski Brod (pronounced [slǎv̞ɔ̝ːnskiː brɔ̝̂ːd]) is a city in eastern Croatia, with a population of 59,000 in 2011. Located in the region of Slavonia, it is the centre of Brod-Posavina County and a river port on the Sava river.
Go to Article

Explanation by Hotspot Model

Slavonski Brod

Slavonski Brod

Slavonski Brod
Slavonski Brod
City
The main square in June 2006

Flag

Coat of arms
Slavonski Brod
Location of Slavonski Brod in Croatia
Coordinates: 45°10′N 18°01′E / 45.167°N 18.017°E / 45.167; 18.017Coordinates: 45°10′N 18°01′E / 45.167°N 18.017°E / 45.167; 18.017
Country  Croatia
County Brod-Posavina
Government
 • Mayor Mirko Duspara (Ind.)
 • City Council
Area
 • City 50.27 km2 (19.41 sq mi)
Elevation 92 m (302 ft)
Population (2011 census)[1]
 • City 59,141
 • Density 1,200/km2 (3,000/sq mi)
 • Metro 80,178
Time zone CET (UTC+1)
 • Summer (DST) CEST (UTC+2)
Postal code 35000
Area code(s) 035
Website Official website

Slavonski Brod (pronounced [slǎv̞ɔ̝ːnskiː brɔ̝̂ːd]) is a city in eastern Croatia, with a population of 59,000 in 2011.[1] Located in the region of Slavonia, it is the centre of Brod-Posavina County and a river port on the Sava river.

Names

Although brod means 'ship' in modern Croatian, the city's name bears witness to an older meaning - 'water crossing', 'ford'.

Among the names historically in use: Marsonia in the Roman Empire, Brood (in Slavonien)[2] in the German speaking Austrian period, Brod na Savi after 1934.

The ancient name "Marsonia" probably comes from the Proto-Indo-European word *mory (marsh), and the same root is seen in the near-by toponyms such as "Mursa" and "Mariniana".[3][unreliable source?]

Geography

The city is located 197 kilometres (122 miles) southeast of Zagreb and at an elevation of 96 metres (315 feet). It developed at the strategically important crossing over the Sava river toward Brod in Bosnia and Herzegovina. The Bosnian city was called Bosanski Brod until 2009.

Slavonski Brod is an important intersection of the Posavina part of the highway and a railway junction, since it is located on the highway linking ZagrebLipovacBelgrade (E70, A3) and the ZagrebVinkovciBelgrade railway. The ship port "Brod" on the Sava river is under construction.

There is also a new modern highway under construction, on the Pan-European Corridor Vc, which will connect Northern Europe and Hungary with Croatia (through the region of Slavonia), and Bosnia and Herzegovina with Croatia (through the coastal region of Dalmatia). The alignment of this highway is approximately at a 19 km (12 mi) distance from the center of the town. With the completion of this route, the area of the town Slavonski Brod will become one of the major highway intersections in this part of Europe connecting directions West-East and North-South.

Demographics

Slavonski Brod is the sixth largest city in Croatia, after Zagreb, Split, Rijeka, Osijek and Zadar.

Brod is the center of a built-up area of more than 110,000 inhabitants including Brod in Bosnia, Sibinj, Bukovlje, Brodski Stupnik, Podcrkavlje, Gornja Vrba and Klakar.

The following settlements comprise the administrative area of Slavonski Brod:[1]

Demography

Historical population
of Slavonski Brod
YearPop.±%
1880 5,872—    
1890 6,940+18.2%
1900 9,627+38.7%
1910 13,193+37.0%
1921 13,729+4.1%
1931 19,203+39.9%
1948 20,196+5.2%
1953 23,116+14.5%
1961 30,093+30.2%
1971 40,043+33.1%
1981 49,153+22.8%
1991 57,229+16.4%
2001 64,612+12.9%
2011 59,141−8.5%
Source: Naselja i stanovništvo Republike Hrvatske 1857–2001, DZS, Zagreb, 2005

A favorable geographical location, pleasant continental climate, fertile soil and vicinity of the river Sava have all resulted with the city being inhabited since a prehistoric age.

History

Prehistory

The northeastern part of the city, at Galovo, recently revealed a rich deposit of the Starčevo culture, dating in the Early Stone Age. Besides the fact that this is the largest architectural finding in northern Croatia, it proves that the locality of Brod has been inhabited for at least 8,000 years.

Roman period

The first historical settlement in Brod dates from Roman times, the settlement being known as Marsonia. It is still disputed whether Marsonia was a postal station, lodging for the night or an actual settlement.

The Peutinger map refers to Marsonia as Marsonie, while the work "Notitia dignitatum" has Marsonia under the name of "Auxilia Ascaria Tauruno sive Marsonia". The issue of Marsonia becoming a city has been tackled by the publishers of Ptolemy's geography, dating from the 16th century. The first geographer who located the position of Marsonia at the locality of Brod was Abraham Ortelius, who, in his atlas Theatrum orbis terrarum (Antwerpen 1590) published a map, the objective of which was to reconstruct and connect the antic names of Panonian and Illyric settlements with the towns of that time. It was he who placed Marsonia at the today's locality of Brod.

The aforementioned Peutinger's table clearly shows that Marsonia initially existed next to the Sava river, at the place where the Roman road crossed the river. The first Croatian expert, claiming that the Roman MARSVNNIA was located where Brod is now is Matija Petar Katančić, giving this assertion additional support.

Before the Yugoslav breakup

The Slavs inhabited the city in the 6th century. The name of the town is mentioned for the first time in Bela IV of Hungary's charter, dated 1224. The Vukovac fortress was built in the 15th century, damaged by the Turks. The Ottoman Empire controlled the settlement from 1536[4] until 1691, when it passed in the Empire of Austria, as confirmed by the Treaty of Karlowitz in 1699. Until 1918, Brod (named Brood before 1850)[5] remained in the Austrian monarchy (Kingdom of Croatia-Slavonia after the compromise of 1867), in the Slavonian Military Frontier, under the administration of the Brooder Grenz-Infanterie-Regiment N°VII until 1881. A huge Vauban type fortress was built east of Vukovac.

Next to its defending role, the city saw development of crafts and trade. The education and culture were strongly dominated by the Franciscans. The 20th century was a period of strong economic growth of the city, with the 1920s being called "the Golden Age of Brod". The city's current name dates from 1934 when it was changed from Brod na Savi.

From 1941 to 1945 the city was part of the Independent State of Croatia. The town was heavily bombed by the Allies in 1944 and 1945. The bombing resulted in damage to 80% of the buildings in Slavonski Brod.[6] The bombing resulted in 897 civilian deaths, 244 military deaths, 208 wounded civilians, and 28 military wounded in Slavonski Brod and Bosanski Brod.[7]

In 1990, democratic reforms legalized the forming of political parties, other than the League of Communists of Croatia. In Slavonski Brod, the first parties formed were the Croatian Democratic Union and the Croatian Democratic Party.[8]

Economy

The city's economy is based on farming, viticulture, fruit growing, metal-processing, timber (furniture wood, parquetry), textiles (ready-made), leather, foodstuffs (brewery), building material (lime), and printing industries.

Slavonski Brod is also home to some of the most important metal companies in Southeastern Europe, the Djuro Djakovic consortium, consisting of a number of factories producing very diverse products, mainly for export. The consortium is capable of producing: locomotives, tramways, wagons, bridges, industrial plants, nuclear reactors, car parts, heavily armed vehicles, armoured fighting vehicles, including main battle tanks and mine warfare vehicles, agricultural machinery, etc.

Service industries are becoming rapidly important, especially tourism. The city has an important cultural heritage, including a fortress and a Franciscan monastery with a rich library.

Cultural heritage

The Brod Fortress from the Baroque period, was constructed during the Austro-Hungarian Empire to serve as a stronghold against the Ottoman Empire, which was situated on the other bank of the Sava river. It is in the Vauban style, named after one of the best European experts in the building of fortifications in 17th and 18th centuries. It is one of Europe's best preserved fortresses, and also one of the biggest on the former Austro-Hungarian Military Frontier. In a way, it is the continental obverse of Diocletian's Palace in Split, by its monumentality.

The city's Franciscan monastery dates from the 18th century, and is also Baroque in style, with exceptional architecture, especially of the church yard, and monastery church interior, with its beautiful altar and paintings. In 1720, a faculty of philosophy was opened here.

The most important annual cultural event in the town is the children's festival 'In the World of the Fairy Tales of Writer Ivana Brlić-Mažuranić', in April and May. The Brodsko kolo, an annual show of original folklore, is held in mid-June, while the Festival of Patriotic Folk Songs takes place in May. The artistic 'Sava' colony\[1] cherishes the tradition of watercolour painting.

One of the attractions of Slavonski Brod is a beautiful central town square, one of the two or three biggest in all of Croatia, Ivana Brlić-Mažuranić square, named after a popular children's writer, whose house is on the square. This square is also home to numerous cultural events and has a perfect view of the beautiful Sava river. The square is also dotted with galleries, book stores, cafes, night clubs, shops etc., which make it perfect place for entertainment. Close to the square, another attraction is the romantic promenade next to the Sava river - 'Kej' as it is called by citizens of town.

Slavonski Brod Synagogue, destroyed during World War II, was among the largest and prestigious synagogues in Croatia.

Slavonski Brod is home to monuments to bishop Josip Stadler and Croatia's first president Franjo Tuđman.[9][10] Slavonski Brod and its rail station are featured in Agatha Christie's Murder on the Orient Express as the place near which the Orient Express breaks down.

Education

Slavonski Brod has very developed educational institutions in pre-school, primary, secondary and high education.

The city also hosts the Faculty of Mechanical Engineering of Osijek University, and the Primary School Teacher Training College. Some other faculties are expected to be opened soon. In October 2006. associate-degree college has been founded with several other faculties.

Surroundings

In the immediate surroundings of the town there are interesting hunting grounds (Migalovci), fishponds (Jelas Polje), and a lake (Petnja). There are pleasant orchards and vineyards, Dilj mountain (or 'Dilj Gora'), and swimming opportunities.

Climate

Climate data for Slavonski Brod (1971–2000, extremes 1963–2014)
Month Jan Feb Mar Apr May Jun Jul Aug Sep Oct Nov Dec Year
Record high °C (°F) 19.4
(66.9)
24.1
(75.4)
27.4
(81.3)
31.4
(88.5)
35.2
(95.4)
37.0
(98.6)
39.5
(103.1)
40.5
(104.9)
36.5
(97.7)
30.2
(86.4)
26.4
(79.5)
23.0
(73.4)
40.5
(104.9)
Average high °C (°F) 3.5
(38.3)
6.9
(44.4)
12.5
(54.5)
17.1
(62.8)
22.2
(72)
25.2
(77.4)
27.4
(81.3)
27.2
(81)
23.1
(73.6)
17.0
(62.6)
9.5
(49.1)
4.8
(40.6)
16.4
(61.5)
Daily mean °C (°F) −0.2
(31.6)
1.9
(35.4)
6.5
(43.7)
11.0
(51.8)
16.1
(61)
19.3
(66.7)
21.0
(69.8)
20.4
(68.7)
16.1
(61)
10.6
(51.1)
5.0
(41)
1.1
(34)
10.7
(51.3)
Average low °C (°F) −3.8
(25.2)
−2.6
(27.3)
0.9
(33.6)
4.9
(40.8)
9.4
(48.9)
12.7
(54.9)
14.0
(57.2)
13.7
(56.7)
9.9
(49.8)
5.4
(41.7)
1.0
(33.8)
−2.4
(27.7)
5.2
(41.4)
Record low °C (°F) −27.8
(−18)
−25.5
(−13.9)
−14.6
(5.7)
−8.4
(16.9)
−1.7
(28.9)
1.7
(35.1)
6.0
(42.8)
4.7
(40.5)
−3.1
(26.4)
−7.4
(18.7)
−13.7
(7.3)
−22
(−8)
−27.8
(−18)
Average precipitation mm (inches) 47.3
(1.862)
38.5
(1.516)
45.8
(1.803)
55.9
(2.201)
69.4
(2.732)
82.4
(3.244)
87.8
(3.457)
67.9
(2.673)
62.9
(2.476)
68.3
(2.689)
68.4
(2.693)
53.4
(2.102)
748.1
(29.453)
Average precipitation days (≥ 0.1 mm) 12.0 11.1 12.1 13.4 12.5 13.8 10.4 10.1 9.7 11.0 12.4 13.7 142.2
Average snowy days (≥ 1.0 cm) 11.2 7.3 1.8 0.2 0.0 0.0 0.0 0.0 0.0 0.0 2.7 7.4 30.6
Average relative humidity (%) 87.1 80.9 73.1 72.0 73.6 74.7 73.7 75.6 79.6 82.4 86.3 88.6 79.0
Mean monthly sunshine hours 55.8 90.4 142.6 174.0 223.2 237.0 269.7 254.2 189.0 130.2 66.0 49.6 1,881.7
Source: Croatian Meteorological and Hydrological Service[11][12]

International relations

Twin towns — Sister cities

Slavonski Brod is twinned with:

See also



This article uses material from the Wikipedia article "Slavonski Brod", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

3D Maps & GIS

3D,Landscape,Maps,Terrain,Profile,LIDAR,Earth,360 Grad,Panorama,GIS,generator,reality,online,Scenes,cartography,topology,Geo,ESRI