powered by CADENAS

Social Share

Head (2322 views - Human)

A head is the part of an organism which usually includes the eyes, ears, nose and mouth, each of which aid in various sensory functions such as sight, hearing, smell, and taste, respectively. Some very simple animals may not have a head, but many bilaterally symmetric forms do. Heads develop in animals by an evolutionary trend known as cephalization. In bilaterally symmetrical animals, nervous tissues concentrate at the anterior region, forming structures responsible for information processing. Through biological evolution, sense organs and feeding structures also concentrate into the anterior region; these collectively form the head.
Go to Article

Explanation by Hotspot Model

Head

Head

Head
The head of a meerkat
Identifiers
TA A01.1.00.001
FMA 7154
Anatomical terminology

A head is the part of an organism which usually includes the eyes, ears, nose and mouth, each of which aid in various sensory functions such as sight, hearing, smell, and taste, respectively. Some very simple animals may not have a head, but many bilaterally symmetric forms do. Heads develop in animals by an evolutionary trend known as cephalization. In bilaterally symmetrical animals, nervous tissues concentrate at the anterior region, forming structures responsible for information processing. Through biological evolution, sense organs and feeding structures also concentrate into the anterior region; these collectively form the head.

Human head

The human head is an anatomical unit that consists of the skull, hyoid bone and cervical vertebrae. The term "skull" collectively denotes the mandible (lower jaw bone) and the cranium (upper portion of the skull that houses the brain). The skull can also be described as being composed of the cranium, which encloses the cranial cavity, and the facial skeleton (includes the mandible). There are eight bones in the cranium and fourteen in the facial skeleton.[1]

Sculptures of human heads are generally based on a skeletal structure that consists of a cranium, jawbone, and cheekbone. Though the number of muscles making up the face is generally consistent between sculptures, the shape of the muscles varies widely based on the function, development, and expressions reflected on the faces of the subjects.[2]

Proponents of identism believe that the mind is identical to the brain. Philosopher John Searle asserts his identist beliefs, stating "the brain is the only thing in the human head". Similarly, Dr. Henry Bennet-Clark has stated that the head encloses billions of "miniagents and microagents (with no single Boss)".[3]

Other animals

The evolution of a head is associated with the cephalization that occurred in Bilateria some 555 million years ago.

Arthropods

In some arthropods, especially trilobites (pictured at right), the cephalon, or cephalic region, is the region of the head which is a collective of "fused segments".[4]

Insects

A typical insect head is composed of eyes, antennae, and components of mouth. As these components differ substantially from insect to insect, they form important identification links. Eyes in the head found, in several types of insects, are in the form of a pair of compound eyes with multiple faces. In many other types of insects the compound eyes are seen in a "single facet or group of single facets". In some case, the eyes may be seen as marks on the dorsal or located near or toward the head, two or three ocelli (single faceted organs).[5]

Antennae on the insect's head is found in the form of segmented attachments, in pairs, that are usually located between the eyes. These are in varying shapes and sizes, in the form of filaments or in different enlarged or clubbed form.[5]

Insects have mouth parts in various shapes depending on their feeding habits. Labrum is the "upper lip" which is in the front area of the head and is the most exterior part. A pair of mandible is found on backside of the labrum flanking the side of the mouth, succeeded by a pair of maxillae each of which is known as maxilliary palp. At the back side of the mouth is the labium or lower lip. There is also an extra mouth part in some insects which is termed as hypopharynx which is usually located between the maxillac.[5]

Vertebrates and the "new head hypothesis"

Though invertebrate chordates – such as the tunicate larvae or the lancelets – have heads, there has been a question of how the vertebrate head, characterized by a bony skull clearly separated from the main body, might have evolved from the head structures of these animals.[6]

According to Hyman (1979), evolution of the head in the vertebrates has occurred by the fusion of a fixed number of anterior segments, in the same manner as in other "heteronomously segmented animals". In some cases segments or a portion of the segments disappear. The head segments also lose most of its systems except for the nervous system. With the progressive development of cephalization, "the head incorporates more and more of the adjacent segments into its structure, so that in general it may be said that the higher the degree of cepahalization the greater is the number of segments composing the head".[7]

In the 1980's, the "new head hypothesis" was proposed, suggesting that the vertebrate head is an evolutionary novelty resulting from the emergence of neural crest and cranial placodes.[8][9] In 2014, a transient larva tissue of the lancelet was found to be virtually indistinguishable from the neural crest-derived cartilage which forms the vertebrate skull, suggesting that persistence of this tissue and expansion into the entire head space could be a viable evolutionary route to formation of the vertebrate head.[6]

In society and culture

Heraldry

The heads of humans and other animals are commonly recurring charges in heraldry.[10] Heads of humans are sometimes blazoned simply as a "man's head", but are far more frequently described in greater detail, either characteristic of a particular race or nationality (such as Moors' heads, Saxons' heads, Egyptians' heads or Turks' heads), or specifically identified (such as the head of Moses in the crest of Hilton, or the head of St. John the Baptist in the crest of the London Company of Tallowchandlers).[10][11] Several varieties of women's heads also occur, including maidens' heads (often couped under the bust, with hair disheveled), ladies' heads, nuns' heads (often veiled), and occasionally queens' heads. The arms of Daveney of Norfolk include "three nun's heads veiled couped at the shoulders proper," and the bust of a queen occurs in the arms of Queenborough, Kent.[10] Infants' or children's heads are often couped at the shoulders with a snake wrapped around the neck (e.g. "Argent, a boy's head proper, crined or, couped below the shoulders, vested gules, garnished gold," in the arms of Boyman).[10]

Art

Study on the proportions of head and eyes by Leonardo da Vinci
"Head of a young man" – Domenico Beccafumi

One of the ways of drawing sketches of heads—as Jack Ham advises—is to develop it in six well defined steps starting with the shape of the head in the shape of an egg. Female head in particular is sketched in a double circle design procedure with proportions considered as ideal of female head. In the first circle division is made of five sections on the diameter, each section of five eyes width. It is then developed over a series of ten defined steps with the smaller circle imposed partially over the larger circle at lower end at the fourth stage. Eyes and chins are fitted in various shapes to form the head.[12]

Leonardo Da Vinci was one of the world’s greatest artists who drew sketches of human anatomy using grid structures. His image of the face drawn on the grid structure principle is in perfect proportion.[13] In this genre, using the technique of pen and ink, Leonardo created a sketch which is a "Study on the proportions of head and eyes”(pictured).[14]

Idiomatic expressions

An idiom is a phrase or a fixed expression that has a figurative, or sometimes literal, meaning.

  • "To come to a head" – to reach a critical stage and require immediate action[15]
  • "To bite someone's head off" – to criticize someone strongly[16]
  • "Can't make head or tail of something" – cannot understand something[17]
  • "A head start" – an early start that provides an advantage over others[18]
  • "Head and shoulders above someone or something" – better than someone or something in some way[19]
  • "To want someone's head on a platter" – to want someone severely punished[20]
  • "To bang your head against a brick wall" – to continually try to achieve something without success[21]
  • "To have one's head in the clouds" – to not pay attention to what is happening around one because one is so absorbed by one's own thoughts[22][23]

Engineering and scientific fields

The head's function and appearance play an analogous role in the etymology of many technical terms. Cylinder head, pothead, and weatherhead are three such examples.

Gallery

See also



This article uses material from the Wikipedia article "Head", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Human

3D