powered by CADENAS

Social Share

Lamborghini Miura (11211 views - Cars & Motorbikes & Trucks)

The Lamborghini Miura is a sports car produced by Italian automaker Lamborghini between 1966 and 1973. The car was possibly the first supercar with a rear mid-engined two-seat layout, although the concept was first pioneered by René Bonnet with the Matra Djet in 1964. This layout has since become the standard for high-performance sports and supercars. When released, it was the fastest production road car made. The Miura was originally conceived by Lamborghini's engineering team, which designed the car in its spare time against the wishes of company founder Ferruccio Lamborghini, who preferred powerful yet sedate grand touring cars over the race car-derived machines produced by local rival Ferrari. The Miura's rolling chassis was presented at the 1965 Turin auto show, and the prototype P400 debuted at the 1966 Geneva show. It received stellar receptions from showgoers and the motoring press alike, each impressed by Marcello Gandini's sleek styling and the car's revolutionary mid-engine design. Lamborghini's flagship, the Miura received periodic updates and remained in production until 1973. A year later the extreme Countach entered the company's lineup, amid tumultuous financial times for the company.
Go to Article

Explanation by Hotspot Model

Lamborghini Miura

Lamborghini Miura

Lamborghini Miura
Overview
Manufacturer Automobili Lamborghini S.p.A
Production 1966–73[1]
764 built
Designer Marcello Gandini at Bertone[2]
Body and chassis
Class Sports car (S)
Body style 2-door coupé
Layout Transverse rear mid-engine, rear-wheel-drive
Powertrain
Engine 3929 cc V12
Transmission 5-speed manual
Dimensions
Wheelbase 2,500 mm (98.4 in)
Length 4,360 mm (171.7 in)
Width 1,760 mm (69.3 in)
Height 1,050 mm (41.3 in)
Curb weight 1,292 kg (2,848 lb)[3]
Chronology
Successor Lamborghini Countach

The Lamborghini Miura is a sports car produced by Italian automaker Lamborghini between 1966 and 1973. The car was possibly the first supercar with a rear mid-engined two-seat layout, although the concept was first pioneered by René Bonnet with the Matra Djet in 1964. This layout has since become the standard for high-performance sports and supercars.[4] When released, it was the fastest production road car made.

The Miura was originally conceived by Lamborghini's engineering team, which designed the car in its spare time against the wishes of company founder Ferruccio Lamborghini, who preferred powerful yet sedate grand touring cars over the race car-derived machines produced by local rival Ferrari.

The Miura's rolling chassis was presented at the 1965 Turin auto show, and the prototype P400 debuted at the 1966 Geneva show. It received stellar receptions from showgoers and the motoring press alike, each impressed by Marcello Gandini's sleek styling and the car's revolutionary mid-engine design.

Lamborghini's flagship, the Miura received periodic updates and remained in production until 1973. A year later the extreme Countach entered the company's lineup, amid tumultuous financial times for the company.

Development

During 1965, Lamborghini's three top engineers, Gian Paolo Dallara, Paolo Stanzani and Bob Wallace put their own time into developing a prototype car known as the P400. The engineers envisioned a road car with racing pedigree, one which could win on the track and be driven on the road by enthusiasts. The three men worked on its design at night, hoping to convince company founder Ferruccio Lamborghini such a vehicle would neither be too expensive nor distract from the company's focus. When finally brought aboard, Lamborghini gave his engineers a free hand in the belief the P400 was a potentially valuable marketing tool, if nothing more.

The car featured a transversely-mounted mid-engine layout, a departure from previous Lamborghini cars. The V12 was also unusual in that it was effectively merged with the transmission and differential, reflecting a lack of space in the tightly-wrapped design. The rolling chassis was displayed at the Turin Salon in 1965. Impressed showgoers placed orders for the car despite the lack of a body to go over the chassis.

Bertone was placed in charge of styling the prototype, which was finished just days before its debut at the 1966 Geneva motor show. None of the engineers had found time to check if the engine fit inside its compartment. Committed to showing the car, they decided to fill the engine bay with ballast and keep the hood locked throughout the show, as they had three years earlier for the début of the 350GTV. Sales head Sgarzi was forced to turn away members of the motoring press who wanted to see the P400's power plant. Despite this setback, the car was the highlight of the show, immediately boosting stylist Marcello Gandini's reputation.

The favourable reaction at Geneva meant the P400 was to go into production by the following year. The name "Miura", after the famous Spanish fighting bull[5] breeder (pronounced [ˈmjuɾa]), was chosen and featured in the company's newly created badge. The car gained the worldwide attention of automotive enthusiasts when it was chosen for the opening sequence of the original 1969 version of The Italian Job. In press interviews of the time Ferruccio Lamborghini was reticent about his precise birth date, but stressed that he was born under the star sign Taurus the bull.[5]

Production history

P400

The earliest model of the Miura was known as the P400 (for Posteriore 4 litri). It was powered by a version of the 3.9 L Lamborghini V12 engine used in the 400GT at the time. The engine was mounted transversely and produced 350 PS (257 kW; 345 hp). Exactly 275 P400 were produced between 1966 and 1969 - a success for Lamborghini despite its then-steep price of US$20,000 (equivalent to $147,631 in 2016).

Taking a cue from the Morris Mini, Lamborghini formed the engine and gearbox in one casting. Its shared lubrication continued until the last 96 SVs, when the case was split to allow the correct oils to be used for each element.

An unconfirmed claim holds the first 125 Miuras were built of 0.9 mm steel and are therefore lighter than later cars. All cars had steel frames and doors, with aluminum front and rear skinned body sections. When leaving the factory they were originally fitted with Pirelli Cinturato 205VR15 tyres (CN72).

Awards

The Miura won the prestigious Gran Turismo Trophy at the 2008 Pebble Beach Concours d'Elegance, and has been re-created for use in the Gran Turismo 5 video game.[6]

P400S

The P400S Miura, also known as the Miura S, made its introduction at the Turin Motorshow in November 1968, where the original chassis had been introduced three years earlier. It was slightly revised from the P400, with the addition of power windows, bright chrome trim around external windows and headlights, new overhead inline console with new rocker switches, engine intake manifolds made 2 mm larger, different camshaft profiles, and notched trunk end panels (allowing for slightly more luggage space). Engine changes were reportedly good for an additional 20 PS (15 kW; 20 hp).

Other revisions were limited to creature comforts, such as a locking glovebox lid, a reversed position of the cigarette lighter and windshield wiper switch, and single release handles for front and rear body sections. Other interior improvements included the addition of power windows and optional air conditioning, available for US$800. About 338 P400S Miura were produced between December 1968 and March 1971. One S #4407 was owned by Frank Sinatra. Miles Davis also owned one, which he crashed in October 1972 under the influence of cocaine, breaking both ankles. Eddie Van Halen owns one and can be heard revving it up during the bridge in the song Panama.

P400SV

The last and most famous Miura, the P400SV or Miura SV was presented in 1971. It featured different cam timing and altered carburetors. These gave the engine an additional 15 PS (11 kW; 15 hp), to 385 PS (283 kW; 380 hp). The last 96 SV engines had a split sump. The gearbox now had its lubrication system separate from the engine, which allowed the use of the appropriate types of oil for the gearbox and the engine. This also alleviated concerns that metal shavings from the gearbox could travel into the engine with disastrous and expensive results and made the application of an optional limited-slip differential far easier.

The SV can be distinguished from its predecessors from its lack of "eyelashes" around the headlamps, wider rear fenders to accommodate the new 9-inch-wide (230 mm) rear wheels and Pirelli Cinturato tires, and different taillights. 150 SVs were produced.

There was a misprint in the SV owners manual indicating bigger intake valves in English size (but correct size in metric). The intake and exhaust valves in all 4 liter V12 Lamborghini remained the same throughout all models. This intake size misprint carried forward into Espada 400GT and Countach LP 400/LP 400S owners manuals as well.

P400 Jota

In 1970, Lamborghini development driver Bob Wallace created a test mule that would conform to the FIA's Appendix J racing regulations. The car was appropriately named the Miura Jota (the pronunciation of the letter 'J' in Spanish). Wallace made extensive modifications to the standard Miura chassis and engine. Weight reductions included replacing steel chassis components and body panels with the lightweight aluminium alloy Avional and replacing side windows with plastic, with the resulting car weighing approximately 800 pounds less than a production Miura.[7] A front spoiler was added and the headlights were replaced with fixed, faired-in units. Wallace substituted two smaller, sill-mounted fuel tanks for the single larger original unit. The suspension was reworked and wider (9" in the front, 12" in the rear), lightweight wheels were fitted. The engine was modified to produce 418-440 bhp at 8800 rpm, with an increased compression ratio, altered cams, electronic ignition, dry-sump lubrication, and less restrictive exhaust system.[8][9] This single example was eventually sold to a private buyer after extensive testing. In April 1971, the car crashed on the yet-unopened ring road around the city of Brescia, and burned to the ground.[10]

It was once widely believed that the Jota had the chassis number of #5084 (a number well out of sequence for the date in question), it has been clarified by Miura expert Joe Sackey in his book The Lamborghini Miura Bible[11] that this is not the case, and that #5084 is in fact a factory modified SV to SVJ spec.

A recreation of the Jota was later undertaken by Chris Lawrence of Wymondham Engineering for Lamborghini owner Piet Pulford from the United Kingdom on chassis #3033.[12]

P400 SV/J

There are six examples of the Miura SV/J known to be built by the factory while the Miura was still in production, one was built new (chassis #5090) and five were converted from existing SVs (chassis #4934, #4860, #4892, #4990 & #5084)

One of these cars, chassis #4934, was built for the Shah of Iran Mohammad Reza Pahlavi.[13] The Shah stored this car under armed guard with another SV in Royal Palace in Tehran. After he fled the country during the Iranian Revolution, his cars were seized by the Iranian government. The SV/J was sold into Dubai in 1995. In 1997 this car was sold in a Brooks auction to Nicolas Cage, at US$490,000, becoming the model's highest ever price at auction.[14] Cage sold the car in 2002. Higher prices have been reached several times since then, including by SVJ #4892 selling for over $1.9M

Of the seven known original cars #4892 is a recent addition to the list of known genuine SVJ's with factory documentation now having come to light.[15][16]

An eighth SV/J was built at the Lamborghini factory between 1983 and 1987 from an unused Miura S chassis. This was made for Jean Claude Mimran, one of the Mimran brothers, the then owner of Lamborghini.[14] Most experts do not recognize this as an "official" SVJ due to it being converted (albeit done by the factory) long after the Miura went out of production.

Further Miuras were subsequently upgraded to SVJ specifications (trying to imitate the real factory SVJs) by various garages of Switzerland, USA and Japan.

Roadster

Another one-off, the Miura Roadster (actually more of a targa-model, but without any removable roof) was built by Bertone as a show car. Based on a P400, it was first shown at the 1968 Brussels Auto Show. After having been exhibited at several auto salons the car was sold to the International Lead Zinc Research Organization (ILZRO) who turned it into a display-vehicle showcasing the possibilities of using zinc alloys in cars. The car was named the ZN75. A few other Miuras have had their tops removed, but this Bertone Miura Roadster was the only factory open-top Miura.

In 2006 the ZN75 was purchased by New York City real estate developer Adam Gordon. Gordon had Bobileff Motorcars in San Diego, California return the car to its original Bertone Roadster form. The restored car was first shown in August 2008 at the Pebble Beach Concours d'Elegance.

The one of a kind Miura Roadster was shown at the Amelia Island Concours d'Elegance in 2013.[17]

P400 SVJ Spider

This one-off example of the Miura was displayed at the 1981 Geneva Motor Show with other new Lamborghini models (Jalpa and LM002) shortly after new company CEO Patrick Mimran took over the factory although it was never a factory authorised model r modifications. Finished in pearl white, the SVJ Spider was the formerly yellow Miura S presented at the 1981 Geneva Motor Show, and uses chassis #4808[18] Equipped with wide wheels and a rear wing reflecting the marque's revival, it was wrongly considered by some as a prototype for a possible limited series of Miura Spider whereas in fact it was simply a one off show car constructed on behalf by the Swiss Lamborghini Importer Lambomotor AG (and as such is not an official factory modification or indeed has any link to the factory bar its original 1970 build).

Subsequently, bought by Swiss Lamborghini collector Jean Wicki, the car had its rear wing and chin spoiler removed and was painted silver, bringing the car's style closer to the Berlinetta SVJ. Lamborghini specialist Autodrome (France) purchased the car from Wicki and restored its bodywork and upholstery in partnership with Carrosserie Lecoq (Paris). Painted traditional Miura lime green, the car was eventually sold to a Parisian collector. The car has stiffness issues and does not drive that well (as described by Miura expert Joe Sackey),[19]

Other than private modifications, there are only two "open" Miuras, officially presented in International Motor shows: the Bertone Miura Roadster, exhibited on Bertone's own stand at Bruxelles in 1968, and this non factory example, shown on the Lamborghini stand at the Geneva Motor show in 1981.

2006 Miura concept

A Miura concept car was presented at the American Museum of Television & Radio on January 5, 2006 alongside the Los Angeles Auto Show, though it was not presented at the show itself. Instead, the Miura concept car officially debuted at the North American International Auto Show two weeks later. It was the first design to be penned by Lamborghini design chief, Walter de'Silva, commemorating the 40th anniversary of the 1966 Geneva introduction of the original Miura.

Lamborghini president and CEO Stefan Winkelmann denied that the concept would mark the Miura's return to production, saying “The Miura was a celebration of our history, but Lamborghini is about the future. Retro design is not what we are here for. So we won’t do the Miura.”[20]

2016 Lamborghini Special edition Aventador Miura Homage

To celebrate the 50th anniversary of the Lamborghini Miura – a forerunner of all V12 Lamborghini super sports cars – Lamborghini has unveiled the Aventador Miura Homage. The special edition car has been created by the company’s Ad Personam customization division.[21]

Specifications

Lamborghini Miura P400 P400S P400SV
Produced:  1966–69
275 built
1968–71
338 built
1971–73
150 built
Engine:  60° 12-cylinder-V engine (four-stroke), mid-mounted
Bore x Stroke:  82 mm (3.2 in) x 62 mm (2.4 in)
Displacement:  3929 cc
Max. Power @ rpm:  350 PS (260 kW; 350 hp) @ 7000 370 PS (270 kW; 360 hp) @ 7700 385 PS (283 kW; 380 hp) @ 7700
Max. Torque @ rpm:  355 N·m (262 lb·ft) @ 5000 388 N·m (286 lb·ft) @ 5500 388 N·m (286 lb·ft) @ 5500
Compression Ratio:  9.5 : 1 10.7 : 1 10.7 : 1
Fuel feed:  Four Weber IDL40 3C 3bbl downdraft carburetors
Valvetrain:  Two overhead camshafts per cylinder bank, chain driven, bucket tappets
Cooling:  liquid
Gearbox:  5-speed-manual & rear wheel drive, ratio 4.083:1
Electrical system:  12 volt
Front suspension:  Upper and lower wishbones, coil springs, stabilizing bar
Rear suspension::  Upper and lower wishbones, coil springs, stabilizing bar
Brakes:  Girling disc brakes all around, hydraulically operated
Steering:  Rack & pinion
Body structure:  Monocoque construction
Dry weight:  1,125 kg (2,480 lb) 1,298 kg (2,862 lb) 1,298 kg (2,862 lb)
Track front/
rear: 
1,400 mm (55 in) 1,400 mm (55 in) 1,400 mm (55 in) 1,400 mm (55 in) 1,400 mm (55 in) 1,540 mm (61 in)
Wheelbase:  2,500 mm (98 in)
Length:  4,360 mm (172 in)
Width:  1,760 mm (69 in) 1,760 mm (69 in) 1,780 mm (70 in)
Height:  1,060 mm (42 in)
Tyre/Tire sizes:  Pirelli Cinturato72 205 VR-15 GR70 VR 15 FR70 HR 15 front, GR70 VR 15 rear
Top speed (measured):  276 km/h (171 mph)
0-60 mph (measured):  7.0 6.7 sec
Fuel Consumption (measured):  21 L/100 km (13 mpg‑imp; 11 mpg‑US)

See also



This article uses material from the Wikipedia article "Lamborghini Miura", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Cars & Motorbikes & Trucks

Car, Truck,MotorBike, Bicycle, Engine, Racer