powered by CADENAS

Social Share

Common external tariff (1496 views - Classification & Specification)

A common external tariff must be introduced when a group of countries forms a customs union. The same customs duties, import quotas, preferences or other non-tariff barriers to trade apply to all goods entering the area, regardless of which country within the area they are entering. It is designed to end re-exportation; but it may also inhibit imports from countries outside the customs union and thereby diminish consumer choice and support protectionism of industries based within the customs union. The common external tariff is a mild form of economic union but may lead to further types of economic integration. In addition to having the same customs duties, the countries may have other common trade policies, such as having the same quotas, preferences or other non-tariff trade regulations apply to all goods entering the area, regardless of which country, within the area, they are entering. Important examples of common external tariff are that of the Mercosur countries (Brazil, Argentina, Venezuela, Paraguay and Uruguay), the Common Customs Tariff of the Eurasian Economic Community customs union as well as the European Union Customs Union.
Go to Article

Common external tariff

Common external tariff

A common external tariff must be introduced when a group of countries forms a customs union. The same customs duties, import quotas, preferences or other non-tariff barriers to trade apply to all goods entering the area, regardless of which country within the area they are entering. It is designed to end re-exportation; but it may also inhibit imports from countries outside the customs union and thereby diminish consumer choice and support protectionism of industries based within the customs union.

The common external tariff is a mild form of economic union but may lead to further types of economic integration. In addition to having the same customs duties, the countries may have other common trade policies, such as having the same quotas, preferences or other non-tariff trade regulations apply to all goods entering the area, regardless of which country, within the area, they are entering.

Important examples of common external tariff are that of the Mercosur countries (Brazil, Argentina, Venezuela, Paraguay and Uruguay), the Common Customs Tariff of the Eurasian Economic Community customs union as well as the European Union Customs Union.

See also



This article uses material from the Wikipedia article "Common external tariff", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Classification & Specification

eclass, ecl@ss, cobie,cibse, unspsc, ominclass, uniclass, taric number