powered by CADENAS

Social Share

Pallet jack (8832 views - Basics)

A pallet jack, also known as a pallet truck, pallet pump, pump truck, dog, or jigger is a tool used to lift and move pallets. Pallet jacks are the most basic form of a forklift and are intended to move heavy or light pallets within a warehouse.
Go to Article

Explanation by Hotspot Model

Pallet jack

Pallet jack

A pallet jack, also known as a pallet truck,[1] pallet pump, pump truck, dog, [1] or jigger[1] is a tool used to lift and move pallets. Pallet jacks are the most basic form of a forklift[2] and are intended to move heavy or light pallets within a warehouse.

Operational principle

The jack is steered by a 'tiller' like lever that also acts as the pump handle for raising the jack. A small handle on the tiller releases the hydraulic fluid, causing the forks to lower. The front wheels inside the end of the forks are mounted on levers attached to linkages that go to levers attached to the jack cylinder. As the hydraulic jack at the 'tiller' end is raised, the links force the wheels down, raising the forks vertically above the front wheels, raising the load upward until it clears the floor. The pallet is only lifted enough to clear the floor for subsequent travel. Oftentimes, pallet jacks are used to move and organize pallets inside a trailer, especially when there is no forklift truck access or availability.

Operating mechanism
Pallet jack in lowered position, allowing it to be inserted under a load on a pallet 
Jack showing how wheels drop, lifting forks and load. The steering tiller and raised hydraulic cylinder are clearly visible on the right 
Underside of a jack showing linkages under forks 

History

Manual pallet jacks have existed since at least 1918.[3] Early types lifted the forks and load only by mechanical linkages. More modern type uses a hand pumped hydraulic jack to lift.

Types

Manual pallet jack

A manual pallet jack is a hand-powered jack. Most commonly seen in retail and personal warehousing operations.

Powered pallet jack

Powered pallet jacks,[4] also known as electric pallet trucks, walkies, single or double pallet jacks, or power jack, are motorized to allow lifting and moving of heavier and stacked pallets. Some contain a platform for the user to stand while moving pallets. The powered pallet jack is generally moved by a throttle on the handle to move forward or in reverse and steered by swinging the handle in the intended direction. Some contain a type of dead man's switch rather than a brake to stop the machine should the user need to stop quickly or leave the machine while it is in use. Others use a system known as "plugging" where in the driver turns the throttle from forward to reverse (or vice versa) to slow and stop the machine, as the dead man's switch is used in emergencies only.

Operational limitations

  • Reversible pallets cannot be used.
  • Double-faced non-reversible pallets cannot have deck-boards where the front wheels extend to the floor.
  • Enables only two-way entry into a four-way notched-stringer pallet, because the forks cannot be inserted into the notches.

Typical dimensions

The North American industry seems to have 'standardized' pallet jacks in several ways:

  • Width of each of two Forks: 7"
  • Fork Width, i.e. The dimension between the outer edges of the forks: Available as 20¼" (51.4 cm) and 27" (68.6 cm)[5]
  • Fork Length: Available as 36" (91.4 cm), 42" (106.7 cm), 48" (122 cm)[5]
  • Lowered Height: 2.9" (7.5 cm)[5]
  • Raised Height: At least 7.5" (19.1),[5] but some will raise higher

In Eurasia the overall dimensions are similar, as modern container palletization has forced standardization in the dimensional domain globally.

See also



This article uses material from the Wikipedia article "Pallet jack", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Basics

3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted