powered by CADENAS

Social Share

Waste container (6484 views - Environmental Protection)

A waste container is a container for temporarily storing waste, and is usually made out of metal or plastic. Some common terms are dustbin, garbage can, and trash can. The words "rubbish", "basket" and "bin" are more common in British English usage; "trash" and "can" are more common in American English usage. "Garbage" may refer to food waste specifically (when distinguished from "trash") or to municipal solid waste in general. In 1875, the first personal rubbish bins were introduced in Britain to create a regulated system of trash collection.
Go to Article

Explanation by Hotspot Model

Waste container

Waste container

Waste container

A waste container is a container for temporarily storing waste, and is usually made out of metal or plastic. Some common terms are dustbin, garbage can, and trash can. The words "rubbish", "basket" and "bin" are more common in British English usage; "trash" and "can" are more common in American English usage. "Garbage" may refer to food waste specifically (when distinguished from "trash") or to municipal solid waste in general. In 1875, the first personal rubbish bins were introduced in Britain to create a regulated system of trash collection. [1]

Curbside dustbins

In many cities and towns, there is a public waste collection service which regularly collects household waste from the curbside. This will be loaded into a garbage truck and driven to a landfill, incinerator or crush facility to be disposed of. Household curbside waste containers are typically either:

  • trash cans, receptacles made of metal or plastic
  • wheelie bins, light, mobile plastic bins[2]

In some areas, each household has multiple bins separated into different categories (usually represented by colours) depending on its suitability for recycling.[3]

Commercial curbside waste containers are often larger dumpsters or skips.

Public litter bins

Public areas, such as parks, often have litter bins placed to improve the social environment by encouraging people not to litter. Such bins in outdoor locations or other busy public areas are usually mounted to the ground or wall to discourage theft, and reduce vandalism, and to improve their appearance are sometimes deliberately artistic or cute.

Metaphors

The term "garbage can" is also used for a model of decision making, the Garbage Can Model of decision making. It is concerned with cases of decision making in great aggregate uncertainty which can cause decisions to arise that from a distant point of view might seem irrational.

A "trash can" metaphor is often used in computer operating system desktop environments as a place files can be moved for deletion.

In a workplace setting, a bin may be euphemistically called "the circular file" or "the round file". Whereas useful documents are filed in a filing cabinet, which is rectangular, junk mail and other worthless items are "filed" in the bin, which is often round.

See also



This article uses material from the Wikipedia article "Waste container", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Environmental Protection

Environment Ecology