powered by CADENAS

Social Share

Lawn mower racing (1643 views - Challenge & Competition & Award)

Lawnmower racing is a form of motorsport in which competitors race modified lawnmowers, usually of the ride-on or self-propelled variety. The original mower engines are retained, but blades are removed for safety. The sport attracts all ages, and is usually entered into in a spirit of fun rather than extreme competitiveness, though many participants do take it seriously.
Go to Article

Lawn mower racing

Lawn mower racing

Lawnmower racing is a form of motorsport in which competitors race modified lawnmowers, usually of the ride-on or self-propelled variety. The original mower engines are retained, but blades are removed for safety. The sport attracts all ages, and is usually entered into in a spirit of fun rather than extreme competitiveness, though many participants do take it seriously.

In the United Kingdom

The sport was independently invented in 1973 in The Cricketers Arms pub in Wisborough Green – not far from the town of Horsham in West Sussex, England, UK – by a group of young men bemoaning the prohibitive costs of getting involved in any kind of motorsport. They formed the British Lawn Mower Racing Association[1] and shortly afterwards, the North West Lawn Mower Racing Association was formed [2] The sport prides itself on being the cheapest motorsport in the world and has become a local event in Sussex.[3]

However, cutting edge research at the University of Nottingham has revealed that in fact the sport may have had a longer history. In 1968, the Ashton on Mersey Cricket Club organised a lawn mower grand prix for the benefit fund of Lancashire cricketer Ken Higgs. The event consisted of a dash over 880 yards and was sponsored by Esso and Player's No. 6 cigarettes. The event was won by Daily Mirror journalist Roy Allett and Jimmy Savile came third. Savile reportedly prayed before competing and remarked that he has never driven a lawn mower before, "How can you mow in a council flat?"[4]

In the United States

The Twelve Mile 500 is a lawn mower race held in the small town of Twelve Mile, Indiana, organized by the Twelve Mile Lions Club and occurring annually on Independence Day. The tradition began in 1963 as a race for factory-built mowers with their mowing decks removed but in 1996 split into a two-race event with one for four-cycle Briggs lawn mowers and another for modified mowers. The race adopted the "Grand Prix" style in 1970 and has been held in Plank Hill Park ever since. The race structure has once again changed with the addition of another race. The 2010 race included a superstock race in addition to the briggs and modified races. The Twelve Mile 500 consists of a 15-mile, 60-lap course run on a quarter-mile track in the park, with a maximum of 33 entrants per race. Each participating team consists of a driver, a two-person pit crew and a lap judge, and must meet a speed of approximately 30 mph to qualify just like in NASCAR racing.

The sport was taken to the United States by the makers of a petrol stabiliser called Sta-bil, who had visited the UK and witnessed a race meeting. It has since grown to have multiple national organizations, including the U.S. Lawn Mower Racing Association and the American Racing Mower Association.

Lawnmower racing should not be confused with go-karting, wherein lawn mower engines have often been used, especially amongst the amateur participants in go-karting. Lawn mower racing is based firmly around the use of both engines and chassis from regular model mowers. Also, where go-karts are exclusively raced on relatively flat surfaces, lawn mowers can be raced off-road.

In North Carolina

Since the summer of 1984, the North Wilkesporo Rotary Club has played host to lawnmower racing at its Wilkes County Agricultural Fairground facility. Sanctioned by the Allegheny Mower Racing Association,[5] oval track racing on the dirt is reminiscent of the beginnings of stock car racing at the North Wilkesboro Speedway and the birth of NASCAR. Crowds have grown from a few hundred to gatherings of thousands on several Saturday nights from June through September. The Wilkes County fairground site is said by many participants to be the premier facility within the AMRA circus.

Proceeds from the club's lawnmower racing events are distributed throughout the year to the many activities supported by the North Wilkesboro Rotary Club. The club contributes to most local United Way agencies, provides annual scholarships to local high school students, holds a Christmas Party for the county's foster children, while also supporting worldwide relief efforts of Rotary International.

In Missouri

Starting in the spring of 2013 lawn mower racing has been held every other Saturday in Patton, Missouri. Racers from all over Southeast Missouri and parts of Arkansas come to the Patton Saddle Club to race their racing machines. The races are held due to a merging of the Southeast Missouri Lawn Mower Racing Association (SMLMRA for short) and the Patton Lions Club. Hundreds of fans come to watch the races at only five dollars a car load. All proceeds are taken care of by the Lions Club.

Racers vary in age from six to seventy in five separate classes. Kids (6–12 years old) run in the Youth Class. Their mowers are limited to a stock lawn mower engine with a governor set to no more than 3650 rpm and a 10:1 gear ratio. Adults classes are split by running time trials. Time trials are set up like a qualifying run in NASCAR. A-Class is the mowers that run the fastest times. D-Class is the mowers that run the slowest during time trials. B and C-Class are in between the other two.

Mowers are unlimited to engine sizes; however, safety is a big role in the rules. All racers are expected to wear full-face helmets, gloves, boots, a long-sleeve racing shirt, and a neck restraint. Mowers must be equipped with back bumpers (no front bumpers), leg protectors where the feet would be on the mower, a kill switch to turn off the engine in case of an accident, working brakes, cupholders, and a plate on the right-hand side of the hood to keep starters from blowing out of the sides if an engine is to blow up.

In New Mexico

Another popular destination for this form of Motorsport is New Mexico. Contrary to other regions, there are strict rules concerning the class of lawnmower as well as the manner in which they are operated. Starting in January of 1983, the lawnmowers used were primarily John Deere, however, due to the dangerous horsepower produced by these engines, this class of lawnmower was no longer found acceptable to race. In 2012, Craftsmen was declared the most used lawnmower brand in New Mexico. Craftsmen had reported 290 racers using this brand in the 127 races in New Mexico that year. Later in 2015 new rules were imposed lied on the lawn mower racing system In New Mexico preventing lawn mower racing to occur in populated locations.

In Australia

Australia's first mower race was dreamt up in a small, country pub in Harrietville, Victoria in 1978. Five men challenged each other to a race around the local hills of the area after an alcohol-related argument. They chugged up the steep slopes belching smoke from their unmodified Briggs & Strattons (popular lawnmower brands), rounded a nominated gum tree, then flew down in "Angel Gear" – Australian outback slang for neutral – to the finish line. "Half the town's 100 people, 300 sheep and 150 dogs were there," according to Brian Ross, six-time president of the Australian Ride-On Lawn Mower Racing Association (AROLMRA) There are also lawn mower racing clubs in the Sunshine Coast, Brisbane, Nowra and Victoria. The first ever national race between all the clubs was held in Dubbo NSW on May 16, 2009.

In popular culture

Notes
  1. ^ BLMRA website
  2. ^ NWLMRA website
  3. ^ "British Lawnmover Racing Association". 
  4. ^ Ernest Dewhurst, 'Cutting a Dash in the Mowing Grand Prix', The Guardian, 7 October 1968, p. 5
  5. ^ http://www.alleghanymowerracingassociation.com/




This article uses material from the Wikipedia article "Lawn mower racing", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Challenge & Competition & Award

Engineering Newcomer - Weekly Challenge - Competition - F1 in School - Formula Student - First