powered by CADENAS

Social Share

Amazon

Sarrus linkage (4468 views - Mechanism & Kinematics)

The Sarrus linkage, invented in 1853 by Pierre Frédéric Sarrus, is a mechanical linkage to convert a limited circular motion to a linear motion without reference guideways. The linkage uses two horizontal plates (red) positioned parallel to each other, one over the other. Two rectangular plates (green) with hinges at the middle connect the horizontal plates. The circular arc motion of a hinge produces a linear vertical movement. The upper plate moves vertically up and down, towards and away from the lower one. The Sarrus linkage is of a three-dimensional class sometimes known as a space crank, unlike the Peaucellier–Lipkin linkage which is a planar mechanism. Although Charles-Nicolas Peaucellier was recognized for being the first to invent such a straight-line mechanism, the Sarrus linkage was invented earlier; it went, however, largely unnoticed.
Go to Article

Youtube


    

Sarrus linkage

Sarrus linkage

The Sarrus linkage, invented in 1853 by Pierre Frédéric Sarrus, is a mechanical linkage to convert a limited circular motion to a linear motion without reference guideways. The linkage uses two horizontal plates (red) positioned parallel to each other, one over the other. Two rectangular plates (green) with hinges at the middle connect the horizontal plates. The circular arc motion of a hinge produces a linear vertical movement. The upper plate moves vertically up and down, towards and away from the lower one. The Sarrus linkage is of a three-dimensional class sometimes known as a space crank, unlike the Peaucellier–Lipkin linkage which is a planar mechanism.

Although Charles-Nicolas Peaucellier was recognized for being the first to invent such a straight-line mechanism, the Sarrus linkage was invented earlier; it went, however, largely unnoticed.[1]

See also



This article uses material from the Wikipedia article "Sarrus linkage", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanism & Kinematics

3D,Geneva double,mechanism,kinematics,rotation,translation