powered by CADENAS

Social Share

Planned obsolescence (5558 views - PLM PDM EDM Dictionary)

Planned obsolescence or built-in obsolescence in industrial design and economics is a policy of planning or designing a product with an artificially limited useful life, so it will become obsolete (that is, unfashionable or no longer functional) after a certain period of time. The rationale behind the strategy is to generate long-term sales volume by reducing the time between repeat purchases (referred to as "shortening the replacement cycle"). Producers that pursue this strategy believe that the additional sales revenue it creates more than offsets the additional costs of research and development and opportunity costs of existing product line cannibalization. In a competitive industry, this is a risky strategy because when consumers catch on to this, they may decide to buy from competitors instead. Planned obsolescence tends to work best when a producer has at least an oligopoly. Before introducing a planned obsolescence, the producer has to know that the consumer is at least somewhat likely to buy a replacement from them. In these cases of planned obsolescence, there is an information asymmetry between the producer – who knows how long the product was designed to last – and the consumer, who does not. When a market becomes more competitive, product lifespans tend to increase. For example, when Japanese vehicles with longer lifespans entered the American market in the 1960s and 1970s, American carmakers were forced to respond by building more durable products. A counterexample is Moore's law, stating that the rather competitive electronic industry plans for double computer capacity every 18 months, and the software industry plan for new program versions that require double computer capacity every 18 months.
Go to Article

Planned obsolescence

Planned obsolescence

Planned obsolescence or built-in obsolescence in industrial design and economics is a policy of planning or designing a product with an artificially limited useful life, so it will become obsolete (that is, unfashionable or no longer functional) after a certain period of time.[1] The rationale behind the strategy is to generate long-term sales volume by reducing the time between repeat purchases (referred to as "shortening the replacement cycle").[2]

Producers that pursue this strategy believe that the additional sales revenue it creates more than offsets the additional costs of research and development and opportunity costs of existing product line cannibalization. In a competitive industry, this is a risky strategy because when consumers catch on to this, they may decide to buy from competitors instead.

Planned obsolescence tends to work best when a producer has at least an oligopoly.[3] Before introducing a planned obsolescence, the producer has to know that the consumer is at least somewhat likely to buy a replacement from them. In these cases of planned obsolescence, there is an information asymmetry between the producer – who knows how long the product was designed to last – and the consumer, who does not. When a market becomes more competitive, product lifespans tend to increase.[citation needed] For example, when Japanese vehicles with longer lifespans entered the American market in the 1960s and 1970s, American carmakers were forced to respond by building more durable products.[4] A counterexample is Moore's law, stating that the rather competitive electronic industry plans for double computer capacity every 18 months, and the software industry plan for new program versions that require double computer capacity every 18 months.[5][clarification needed]

History and origins of the phrase

In the United States, automotive design reached a turning point in 1924 when the American national automobile market began reaching saturation. To maintain unit sales, General Motors head Alfred P. Sloan Jr. suggested annual model-year design changes to convince car owners that they needed to buy a new replacement each year, an idea borrowed from the bicycle industry, though the concept is often misattributed to Sloan.[7] Critics called his strategy "planned obsolescence". Sloan preferred the term "dynamic obsolescence". This strategy had far-reaching effects on the auto business, the field of product design, and eventually the American economy. The smaller players could not maintain the pace and expense of yearly re-styling. Henry Ford did not like the model-year change because he clung to an engineer's notions of simplicity, economies of scale, and design integrity. GM surpassed Ford's sales in 1931 and became the dominant company in the industry thereafter. The frequent design changes also made it necessary to use a body-on-frame rather than the lighter, but less flexible,[clarification needed] unibody design used by most European automakers.

The origins of phrase, planned obsolescence, go back at least as far as 1932 with Bernard London's pamphlet Ending the Depression Through Planned Obsolescence.[8] The essence of London's plan would have the government impose a legal obsolescence on consumer articles, to stimulate and perpetuate consumption.

However, the phrase was first popularized in 1954 by Brooks Stevens, an American industrial designer. Stevens was due to give a talk at an advertising conference in Minneapolis in 1954. Without giving it much thought, he used the term as the title of his talk. From that point on, "planned obsolescence" became Stevens' catchphrase. By his definition, planned obsolescence was "Instilling in the buyer the desire to own something a little newer, a little better, a little sooner than is necessary."

The phrase was quickly taken up by others, but Stevens' definition was challenged. By the late 1950s, planned obsolescence had become a commonly used term for products designed to break easily or to quickly go out of style. In fact, the concept was so widely recognized that in 1959 Volkswagen mocked it in an advertising campaign. While acknowledging the widespread use of planned obsolescence among automobile manufacturers, Volkswagen pitched itself as an alternative. "We do not believe in planned obsolescence", the ads suggested. "We don't change a car for the sake of change."[9] In the famous Volkswagen advertising campaign by Doyle Dane Bernbach, one advert showed an almost blank page with the strapline "No point in showing the 1962 Volkswagen, it still looks the same".

In 1960, cultural critic Vance Packard published The Waste Makers, promoted as an exposé of "the systematic attempt of business to make us wasteful, debt-ridden, permanently discontented individuals".

Packard divided planned obsolescence into two sub categories: obsolescence of desirability and obsolescence of function. "Obsolescence of desirability", also called "psychological obsolescence", referred to marketers' attempts to wear out a product in the owner's mind. Packard quoted industrial designer George Nelson, who wrote: "Design... is an attempt to make a contribution through change. When no contribution is made or can be made, the only process available for giving the illusion of change is 'styling!'"

Types

Contrived durability

Contrived durability is a strategy of shortening the product lifetime before it is released onto the market, by designing it to deteriorate quickly.[3] The design of all consumer products includes an expected average lifetime permeating all stages of development. Thus, it must be decided early in the design of a complex product how long it is designed to last so that each component can be made to those specifications. Since all matter is subject to entropy, it is impossible for any designed object to retain its full function forever; all products will ultimately break down, no matter what steps are taken. While it is known that products are optimized to match their required lifespan, such designs are often chosen for cost or weight saving reasons. Limited lifespan is only a sign of planned obsolescence if the lifespan of the product is rendered artificially short by design.

The strategy of contrived durability is generally not prohibited by law, and manufacturers are free to set the durability level of their products.[3]

A possible method of limiting a product's durability is to use inferior materials in critical areas, or suboptimal component layouts which cause excessive wear. Using soft metal in screws and cheap plastic instead of metal in stress-bearing components will increase the speed at which a product will become inoperable through normal usage and render it prone to breakage from even minor forms of abnormal usage. For example, small, brittle plastic gears in toys are extremely prone to damage if the toy is played with roughly, which can easily destroy key functions of the toy and force the purchase of a replacement. The short life expectancy of smartphones and other handheld electronics is a result of constant usage, fragile batteries, and the ability to easily damage them. [10]

Prevention of repairs

The ultimate examples of such design are single-use versions of traditionally durable goods, such as disposable cameras, where the customer must purchase an entire new product after using them a single time. Such products are often designed to be impossible to service; for example, a cheap "throwaway" digital watch may have a casing which is simply sealed in the factory, with no designed ability for the user to access the interior without destroying the watch entirely.

Even high-end products may contain design features meant to frustrate repairs, such as "tamper-resistant" screws that use an obscure or proprietary design—a practice infamously adopted by Apple.[12] Front loading washing machines often have the drum bearing - a critical and wear-prone mechanical component - permanently molded into the wash tub, making it impossible to renew without replacing the entire tub, the cost of which usually exceeds the residual value of the appliance, forcing its scrappage.[13][14]

According to Kyle Wiens, co-founder of an online repair community, a possible goal for such design is to make the cost of repairs comparable to the replacement cost, or to prevent any form of servicing of the product at all. In 2012, Toshiba was criticized for issuing cease-and-desist letters to the owner of a website that hosted its copyrighted repair manuals, to the detriment of the independent and home repair market.[15]

Some products, such as Apple mobile devices, contain batteries that are not user-replaceable after they have worn down. While such a design can help make the device thinner, it also makes it difficult to replace the battery without sending the entire device away for repairs or purchasing a replacement (whereupon the original item then becomes waste that must be disposed of).[16]

Perceived obsolescence

Obsolescence of desirability or stylistic obsolescence occurs when designers change the styling of products so customers will purchase products more frequently due to the decrease in the perceived desirability of unfashionable items.

Many products are primarily desirable for aesthetic rather than functional reasons. An obvious example of such a product is clothing. Such products experience a cycle of desirability referred to as a "fashion cycle". By continually introducing new aesthetics, and retargeting or discontinuing older designs, a manufacturer can "ride the fashion cycle", allowing for constant sales despite the original products remaining fully functional. Sneakers are popular fashion industry where this is prevalent - Nike's Air Max line of running shoes is a prime example where a single model of shoe is often produced for years, but the color and material combination ("colorway") is changed every few months, or different colorways are offered in different markets. This has the upshot of ensuring constant demand for the product, even though it remains fundamentally the same.

To a more limited extent this is also true of some consumer electronic products, where manufacturers will release slightly updated products at regular intervals and emphasize their value as status symbols.

Systemic obsolescence

Planned systemic obsolescence is the deliberate attempt to make a product obsolete by altering the system in which it is used in such a way as to make its continued use difficult. Common examples of planned systemic obsolescence include not accommodating forward compatibility in software, or routinely changing screws or fasteners so that they cannot easily be operated on with existing tools. Another example of a company that practices this is Apple Inc. “Apple designs the new operating systems, which have more features, take up more space and require more computing power, for the new iPhones. In order for those apps to remain relevant and keep working, developers have to update them to work with Apple’s latest software and hardware.” [17] Apple constantly urges app designers to produce apps that are suited with the newest created operating system. The software old iPhones obtain purposely lack compatibility with new iPhone software, preventing the user from successfully upgrading their phone.

Programmed obsolescence

In some cases, notification may be combined with the deliberate disabling of a product to prevent it from working, thus requiring the buyer to purchase a replacement. Example: inkjet printer manufacturers that employ smart chips in their ink cartridges to prevent them from being used after a certain threshold (number of pages, time, etc.), even though the cartridge may still contain usable ink or could be refilled (with ink toners, up to 50 percent of the toner cartridge is often still full[18]). This constitutes "programmed obsolescence", in that there is no random component contributing to the decline in function. In the Jackie Blennis v. HP class action suit, it was claimed that Hewlett Packard designed certain inkjet printers and cartridges to shut down on an undisclosed expiration date, and at this point consumers were prevented from using the ink that remained in the expired cartridge. HP denied these claims, but agreed to discontinue the use of certain messages, and to make certain changes to the disclosures on its website and packaging, as well as compensating affected consumers with a total credit of up to $5,000,000 for future purchases from HP.[19] Samsung produces printers that are programmed to stop working even though the printer is still working perfectly. There are some work-arounds for users, for instance to more than double the life of the printer after it stops with a message to replace the imaging drum.[20]

Advantages and disadvantages

Estimates of planned obsolescence can influence a company's decisions about product engineering. Therefore, the company can use the least expensive components that satisfy product lifetime projections.

Also, for industries, planned obsolescence stimulates demand by encouraging purchasers/putting them under pressure to buy sooner if they still want a functioning product. These products can be bought from the same manufacturer (a replacement part or a newer model), or from a competitor who might also rely on planned obsolescence. Especially in developed countries (where many industries already face a saturated market), this technique is often necessary for producers to maintain their level of revenue.

While planned obsolescence is appealing to producers, it can also do significant harm to the society in the form of negative externalities. Continuously replacing, rather than repairing, products creates more waste and pollution, uses more natural resources, and results in more consumer spending. Planned obsolescence can thus have a negative impact on the environment in aggregate. Even when planned obsolescence might help to save scarce resources per unit produced, it tends to increase output in aggregate, since due to laws of supply and demand decreases in cost and price will eventually result in increases in demand and consumption. However, the negative environmental impacts of planned obsolescence are dependent also on the process of production.[21]

There is also the potential backlash of consumers who learn that the manufacturer invested money to make the product obsolete faster; such consumers might turn to a producer (if any exists) that offers a more durable alternative.

Regulation

In 2015, as part of a larger movement against planned obsolescence across the European Union, France has passed legislation requiring that appliance manufacturers and vendors declare the intended product lifespans, and to inform consumers how long spare parts for a given product will be produced. From 2016, appliance manufacturers are required to repair or replace, free of charge, any defective product within two years from its original purchase date. This effectively creates a mandatory two-year warranty.[22]

Critics and supporters

Shortening the replacement cycle has critics and supporters.

Philip Kotler argues that: "Much so-called planned obsolescence is the working of the competitive and technological forces in a free society—forces that lead to ever-improving goods and services."[23]

Critics such as Vance Packard claim the process wastes and exploits customers. With psychological obsolescence, resources are used up making changes, often cosmetic changes, that are not of great value to the customer. Miles Park advocates new and collaborative approaches between the designer and the consumer to challenge obsolescence in fast-moving sectors such as consumer electronics [24]

Some people, such as Ronny Balcaen, have proposed to create a new label to counter the diminishing quality of products due to the planned obsolescence technique.[18]

In software

Software companies sometimes deliberately drop support for older technologies as a calculated attempt to force users to purchase new products to replace those made obsolete.[25] Most proprietary software will ultimately reach an end-of-life point - usually because the cost of support exceeds the revenue generated by supporting the old version - at which the supplier will cease updates and support. As free software and open source software can always be updated and maintained by somebody else, the user is not at the sole mercy of a proprietary vendor.[26] Software which is abandoned by the manufacturer with regard to manufacturer support is sometimes called abandonware.

In academia

Russell Jacoby, writing in the 1970s, observes that intellectual production has succumbed to the same pattern of planned obsolescence used by manufacturing enterprises to generate ever-renewed demand for their products.

The application of planned obsolescence to thought itself has the same merit as its application to consumer goods; the new is not only shoddier than the old, it fuels an obsolete social system that staves off its replacement by manufacturing the illusion that it is perpetually new.[27]

Camille Paglia characterizes contemporary academic discourse influenced by French theorists such as Lacan, Derrida, and Foucault as the academic equivalent of name brand consumerism. "Lacan, Derrida, and Foucault," she says, "are the academic equivalents of BMW, Rolex, and Cuisinart."[28] Under the inspiration of the latest academic fashions, academic planned obsolescence is to manufacture content with little merit for the same reason fashion designers come out with new fashions.

Future

Planned obsolescence has been assumed a necessity when it comes to stimulating consumption; however, this practice has come into question. In 2015 the French Assembly established a fine of up to 300,000 euros and jail terms of up to two years for those manufacturers planning the death of their products in advance. The rule is not only relevant because of the sanctions that it establishes but also because it is the first time that a legislation recognizes openly the existence of planned obsolescence. These techniques may include "a deliberate introduction of a flaw, a weakness, a scheduled stop, a technical limitation, incompatibility or other obstacles for repair", reads the text regarding what may be considered as planned obsolescence.

The European Union is also beginning to address this problem. The European Economic and Social Committee (EESC), an advisory body of the EU,[29] announced in 2013 that it was studying "a total ban on planned obsolescence". It said replacing products that are designed to stop working within two or three years of their purchase was a waste of energy and resources and generated pollution.[30] The EESC organised a round table in Madrid in 2014 on 'Best practices in the domain of built-in obsolescence and collaborative consumption' which called for sustainable consumption to be enshrined as a consumer right in EU legislation.[31] Carlos Trias Pinto, president of the EESC's Consultative Commission on Industrial Change[32] supports "the introduction of a labeling system which indicates the durability of a device, so the consumer has the possibility of choosing whether he/she prefers to buy a cheap product or a more expensive, more durable product".[33]

See also



This article uses material from the Wikipedia article "Planned obsolescence", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

PLM PDM EDM Dictionary

3d,plm,pdm,edm