powered by CADENAS

Social Share

Stereoscopy (8594 views - CAD CAM (Mechanical) Dictionary)

Stereoscopy (also called stereoscopics, or stereo imaging) is a technique for creating or enhancing the illusion of depth in an image by means of stereopsis for binocular vision. The word stereoscopy derives from Greek στερεός (stereos), meaning 'firm, solid', and σκοπέω (skopeō), meaning 'to look, to see'. Any stereoscopic image is called a stereogram. Originally, stereogram referred to a pair of stereo images which could be viewed using a stereoscope. Most stereoscopic methods present two offset images separately to the left and right eye of the viewer. These two-dimensional images are then combined in the brain to give the perception of 3D depth. This technique is distinguished from 3D displays that display an image in three full dimensions, allowing the observer to increase information about the 3-dimensional objects being displayed by head and eye movements.
Go to Article

Explanation by Hotspot Model

Stereoscopy

Stereoscopy

Stereoscopy (also called stereoscopics, or stereo imaging) is a technique for creating or enhancing the illusion of depth in an image by means of stereopsis for binocular vision. The word stereoscopy derives from Greek στερεός (stereos), meaning 'firm, solid', and σκοπέω (skopeō), meaning 'to look, to see'.[2][3] Any stereoscopic image is called a stereogram. Originally, stereogram referred to a pair of stereo images which could be viewed using a stereoscope.

Most stereoscopic methods present two offset images separately to the left and right eye of the viewer. These two-dimensional images are then combined in the brain to give the perception of 3D depth. This technique is distinguished from 3D displays that display an image in three full dimensions, allowing the observer to increase information about the 3-dimensional objects being displayed by head and eye movements.

Background

Stereoscopy creates the illusion of three-dimensional depth from given two-dimensional images.[4] Human vision, including the perception of depth, is a complex process, which only begins with the acquisition of visual information taken in through the eyes; much processing ensues within the brain, as it strives to make sense of the raw information. One of the functions that occur within the brain as it interprets what the eyes see is assessing the relative distances of objects from the viewer, and the depth dimension of those objects. The cues that the brain uses to gauge relative distances and depth in a perceived scene include[5]

  • Stereopsis
  • Accommodation of the eye
  • Overlapping of one object by another
  • Subtended visual angle of an object of known size
  • Linear perspective (convergence of parallel edges)
  • Vertical position (objects closer to the horizon in the scene tend to be perceived as farther away)
  • Haze or contrast, saturation, and color, greater distance generally being associated with greater haze, desaturation, and a shift toward blue
  • Change in size of textured pattern detail

(All but the first two of the above cues exist in traditional two-dimensional images, such as paintings, photographs, and television.)[6]

Stereoscopy is the production of the illusion of depth in a photograph, movie, or other two-dimensional image by the presentation of a slightly different image to each eye, which adds the first of these cues (stereopsis). The two images are then combined in the brain to give the perception of depth. Because all points in the image produced by stereoscopy focus at the same plane regardless of their depth in the original scene, the second cue, focus, is not duplicated and therefore the illusion of depth is incomplete. There are also mainly two effects of stereoscopy that are unnatural for human vision: (1) the mismatch between convergence and accommodation, caused by the difference between an object's perceived position in front of or behind the display or screen and the real origin of that light; and (2) possible crosstalk between the eyes, caused by imperfect image separation in some methods of stereoscopy.

Although the term "3D" is ubiquitously used, the presentation of dual 2D images is distinctly different from displaying an image in three full dimensions. The most notable difference is that, in the case of "3D" displays, the observer's head and eye movement do not change the information received about the 3-dimensional objects being viewed. Holographic displays and volumetric display do not have this limitation. Just as it is not possible to recreate a full 3-dimensional sound field with just two stereophonic speakers, it is an overstatement to call dual 2D images "3D". The accurate term "stereoscopic" is more cumbersome than the common misnomer "3D", which has been entrenched by many decades of unquestioned misuse. Although most stereoscopic displays do not qualify as real 3D display, all real 3D displays are also stereoscopic displays because they meet the lower criteria also.

Most 3D displays use this stereoscopic method to convey images. It was first invented by Sir Charles Wheatstone in 1838,[7][8] and improved by Sir David Brewster who made the first portable 3D viewing device.[9]

Wheatstone originally used his stereoscope (a rather bulky device)[10] with drawings because photography was not yet available, yet his original paper seems to foresee the development of a realistic imaging method:[11]

For the purposes of illustration I have employed only outline figures, for had either shading or colouring been introduced it might be supposed that the effect was wholly or in part due to these circumstances, whereas by leaving them out of consideration no room is left to doubt that the entire effect of relief is owing to the simultaneous perception of the two monocular projections, one on each retina. But if it be required to obtain the most faithful resemblances of real objects, shadowing and colouring may properly be employed to heighten the effects. Careful attention would enable an artist to draw and paint the two component pictures, so as to present to the mind of the observer, in the resultant perception, perfect identity with the object represented. Flowers, crystals, busts, vases, instruments of various kinds, &c., might thus be represented so as not to be distinguished by sight from the real objects themselves.[7]

Stereoscopy is used in photogrammetry and also for entertainment through the production of stereograms. Stereoscopy is useful in viewing images rendered from large multi-dimensional data sets such as are produced by experimental data. Modern industrial three-dimensional photography may use 3D scanners to detect and record three-dimensional information.[12] The three-dimensional depth information can be reconstructed from two images using a computer by correlating the pixels in the left and right images.[13] Solving the Correspondence problem in the field of Computer Vision aims to create meaningful depth information from two images.

Visual requirements

Anatomically, there are 3 levels of binocular vision required to view stereo images:

  1. Simultaneous perception
  2. Fusion (binocular 'single' vision)
  3. Stereopsis

These functions develop in early childhood. Some people who have strabismus disrupt the development of stereopsis, however orthoptics treatment can be used to improve binocular vision. A person's stereoacuity determines the minimum image disparity they can perceive as depth. It is believed that approximately 12% of people are unable to properly see 3D images, due to a variety of medical conditions.[14][15] According to another experiment up to 30% of people have very weak stereoscopic vision preventing them from depth perception based on stereo disparity. This nullifies or greatly decreases immersion effects of stereo to them.[16]

Stereoscopic viewing may be artificially created by the viewer's brain, as demonstrated with the Van Hare Effect, where the brain perceives stereo images even when the paired photographs are identical. This "false dimensionality" results from the developed stereoacuity in the brain, allowing the viewer to fill in depth information even when few if any 3D cues are actually available in the paired images.

Side-by-side

Traditional stereoscopic photography consists of creating a 3D illusion starting from a pair of 2D images, a stereogram. The easiest way to enhance depth perception in the brain is to provide the eyes of the viewer with two different images, representing two perspectives of the same object, with a minor deviation equal or nearly equal to the perspectives that both eyes naturally receive in binocular vision.

To avoid eyestrain and distortion, each of the two 2D images should be presented to the viewer so that any object at infinite distance is perceived by the eye as being straight ahead, the viewer's eyes being neither crossed nor diverging. When the picture contains no object at infinite distance, such as a horizon or a cloud, the pictures should be spaced correspondingly closer together.

The principal advantages of side-by-side viewers is the lack of diminution of brightness, allowing the presentation of images at very high resolution and in full spectrum color, simplicity in creation, and little or no additional image processing is required. Under some circumstances, such as when a pair of images are presented for freeviewing, no device or additional optical equipment is needed.

The principal disadvantage of side-by-side viewers is that large image displays are not practical and resolution is limited by the lesser of the display medium or human eye. This is because as the dimensions of an image are increased, either the viewing apparatus or viewer themselves must move proportionately further away from it in order to view it comfortably. Moving closer to an image in order to see more detail would only be possible with viewing equipment that adjusted to the difference.

Freeviewing

Freeviewing is viewing a side-by-side image pair without using a viewing device.[17]

Two methods are available to freeview:[18][19]

  • The parallel viewing method uses an image pair with the left-eye image on the left and the right-eye image on the right. The fused three-dimensional image appears larger and more distant than the two actual images, making it possible to convincingly simulate a life-size scene. The viewer attempts to look through the images with the eyes substantially parallel, as if looking at the actual scene. This can be difficult with normal vision because eye focus and binocular convergence are habitually coordinated. One approach to decoupling the two functions is to view the image pair extremely close up with completely relaxed eyes, making no attempt to focus clearly but simply achieving comfortable stereoscopic fusion of the two blurry images by the "look-through" approach, and only then exerting the effort to focus them more clearly, increasing the viewing distance as necessary. Regardless of the approach used or the image medium, for comfortable viewing and stereoscopic accuracy the size and spacing of the images should be such that the corresponding points of very distant objects in the scene are separated by the same distance as the viewer's eyes, but not more; the average interocular distance is about 63 mm. Viewing much more widely separated images is possible, but because the eyes never diverge in normal use it usually requires some previous training and tends to cause eye strain.
  • The cross-eyed viewing method swaps the left and right eye images so that they will be correctly seen cross-eyed, the left eye viewing the image on the right and vice versa. The fused three-dimensional image appears to be smaller and closer than the actual images, so that large objects and scenes appear miniaturized. This method is usually easier for freeviewing novices. As an aid to fusion, a fingertip can be placed just below the division between the two images, then slowly brought straight toward the viewer's eyes, keeping the eyes directed at the fingertip; at a certain distance, a fused three-dimensional image should seem to be hovering just above the finger. Alternatively, a piece of paper with a small opening cut into it can be used in a similar manner; when correctly positioned between the image pair and the viewer's eyes, it will seem to frame a small three-dimensional image.

Prismatic, self-masking glasses are now being used by some cross-eyed-view advocates. These reduce the degree of convergence required and allow large images to be displayed. However, any viewing aid that uses prisms, mirrors or lenses to assist fusion or focus is simply a type of stereoscope, excluded by the customary definition of freeviewing.

Stereoscopically fusing two separate images without the aid of mirrors or prisms while simultaneously keeping them in sharp focus without the aid of suitable viewing lenses inevitably requires an unnatural combination of eye vergence and accommodation. Simple freeviewing therefore cannot accurately reproduce the physiological depth cues of the real-world viewing experience. Different individuals may experience differing degrees of ease and comfort in achieving fusion and good focus, as well as differing tendencies to eye fatigue or strain.

Autostereogram

An autostereogram is a single-image stereogram (SIS), designed to create the visual illusion of a three-dimensional (3D) scene within the human brain from an external two-dimensional image. In order to perceive 3D shapes in these autostereograms, one must overcome the normally automatic coordination between focusing and vergence.

Stereoscope and stereographic cards

The stereoscope is essentially an instrument in which two photographs of the same object, taken from slightly different angles, are simultaneously presented, one to each eye. A simple stereoscope is limited in the size of the image that may be used. A more complex stereoscope uses a pair of horizontal periscope-like devices, allowing the use of larger images that can present more detailed information in a wider field of view.

Transparency viewers

Some stereoscopes are designed for viewing transparent photographs on film or glass, known as transparencies or diapositives and commonly called slides. Some of the earliest stereoscope views, issued in the 1850s, were on glass. In the early 20th century, 45x107 mm and 6x13 cm glass slides were common formats for amateur stereo photography, especially in Europe. In later years, several film-based formats were in use. The best-known formats for commercially issued stereo views on film are Tru-Vue, introduced in 1931, and View-Master, introduced in 1939 and still in production. For amateur stereo slides, the Stereo Realist format, introduced in 1947, is by far the most common.

Head-mounted displays

The user typically wears a helmet or glasses with two small LCD or OLED displays with magnifying lenses, one for each eye. The technology can be used to show stereo films, images or games, but it can also be used to create a virtual display. Head-mounted displays may also be coupled with head-tracking devices, allowing the user to "look around" the virtual world by moving their head, eliminating the need for a separate controller. Performing this update quickly enough to avoid inducing nausea in the user requires a great amount of computer image processing. If six axis position sensing (direction and position) is used then wearer may move about within the limitations of the equipment used. Owing to rapid advancements in computer graphics and the continuing miniaturization of video and other equipment these devices are beginning to become available at more reasonable cost.

Head-mounted or wearable glasses may be used to view a see-through image imposed upon the real world view, creating what is called augmented reality. This is done by reflecting the video images through partially reflective mirrors. The real world view is seen through the mirrors' reflective surface. Experimental systems have been used for gaming, where virtual opponents may peek from real windows as a player moves about. This type of system is expected to have wide application in the maintenance of complex systems, as it can give a technician what is effectively "x-ray vision" by combining computer graphics rendering of hidden elements with the technician's natural vision. Additionally, technical data and schematic diagrams may be delivered to this same equipment, eliminating the need to obtain and carry bulky paper documents.

Augmented stereoscopic vision is also expected to have applications in surgery, as it allows the combination of radiographic data (CAT scans and MRI imaging) with the surgeon's vision.

Virtual retinal displays

A virtual retinal display (VRD), also known as a retinal scan display (RSD) or retinal projector (RP), not to be confused with a "Retina Display", is a display technology that draws a raster image (like a television picture) directly onto the retina of the eye. The user sees what appears to be a conventional display floating in space in front of them. For true stereoscopy, each eye must be provided with its own discrete display. To produce a virtual display that occupies a usefully large visual angle but does not involve the use of relatively large lenses or mirrors, the light source must be very close to the eye. A contact lens incorporating one or more semiconductor light sources is the form most commonly proposed. As of 2013, the inclusion of suitable light-beam-scanning means in a contact lens is still very problematic, as is the alternative of embedding a reasonably transparent array of hundreds of thousands (or millions, for HD resolution) of accurately aligned sources of collimated light.

3D viewers

There are two categories of 3D viewer technology, active and passive. Active viewers have electronics which interact with a display. Passive viewers filter constant streams of binocular input to the appropriate eye.

Active

Shutter systems

A shutter system works by openly presenting the image intended for the left eye while blocking the right eye's view, then presenting the right-eye image while blocking the left eye, and repeating this so rapidly that the interruptions do not interfere with the perceived fusion of the two images into a single 3D image. It generally uses liquid crystal shutter glasses. Each eye's glass contains a liquid crystal layer which has the property of becoming dark when voltage is applied, being otherwise transparent. The glasses are controlled by a timing signal that allows the glasses to alternately darken over one eye, and then the other, in synchronization with the refresh rate of the screen. The main drawback of active shutters is that most 3D videos and movies were shot with simultaneous left and right views, so that it introduces a "time parallax" for anything side-moving: for instance, someone walking at 3.4 mph will be seen 20% too close or 25% too remote in the most current case of a 2x60 Hz projection.

Passive

Polarization systems

To present stereoscopic pictures, two images are projected superimposed onto the same screen through polarizing filters or presented on a display with polarized filters. For projection, a silver screen is used so that polarization is preserved. On most passive displays every other row of pixels are polarized for one eye or the other.[20] This method is also known as being interlaced. The viewer wears low-cost eyeglasses which also contain a pair of opposite polarizing filters. As each filter only passes light which is similarly polarized and blocks the opposite polarized light, each eye only sees one of the images, and the effect is achieved.

Interference filter systems

This technique uses specific wavelengths of red, green, and blue for the right eye, and different wavelengths of red, green, and blue for the left eye. Eyeglasses which filter out the very specific wavelengths allow the wearer to see a full color 3D image. It is also known as spectral comb filtering or wavelength multiplex visualization or super-anaglyph. Dolby 3D uses this principle. The Omega 3D/Panavision 3D system has also used an improved version of this technology[21] In June 2012 the Omega 3D/Panavision 3D system was discontinued by DPVO Theatrical, who marketed it on behalf of Panavision, citing ″challenging global economic and 3D market conditions″.[22]

Color anaglyph systems

Anaglyph 3D is the name given to the stereoscopic 3D effect achieved by means of encoding each eye's image using filters of different (usually chromatically opposite) colors, typically red and cyan. Red-cyan filters can be used because our vision processing systems use red and cyan comparisons, as well as blue and yellow, to determine the color and contours of objects. Anaglyph 3D images contain two differently filtered colored images, one for each eye. When viewed through the "color-coded" "anaglyph glasses", each of the two images reaches one eye, revealing an integrated stereoscopic image. The visual cortex of the brain fuses this into perception of a three dimensional scene or composition.[23]

Chromadepth system

The ChromaDepth procedure of American Paper Optics is based on the fact that with a prism, colors are separated by varying degrees. The ChromaDepth eyeglasses contain special view foils, which consist of microscopically small prisms. This causes the image to be translated a certain amount that depends on its color. If one uses a prism foil now with one eye but not on the other eye, then the two seen pictures – depending upon color – are more or less widely separated. The brain produces the spatial impression from this difference. The advantage of this technology consists above all of the fact that one can regard ChromaDepth pictures also without eyeglasses (thus two-dimensional) problem-free (unlike with two-color anaglyph). However the colors are only limitedly selectable, since they contain the depth information of the picture. If one changes the color of an object, then its observed distance will also be changed.[citation needed]

Pulfrich method

The Pulfrich effect is based on the phenomenon of the human eye processing images more slowly when there is less light, as when looking through a dark lens. Because the Pulfrich effect depends on motion in a particular direction to instigate the illusion of depth, it is not useful as a general stereoscopic technique. For example, it cannot be used to show a stationary object apparently extending into or out of the screen; similarly, objects moving vertically will not be seen as moving in depth. Incidental movement of objects will create spurious artifacts, and these incidental effects will be seen as artificial depth not related to actual depth in the scene.

Over/under format

Stereoscopic viewing is achieved by placing an image pair one above one another. Special viewers are made for over/under format that tilt the right eyesight slightly up and the left eyesight slightly down. The most common one with mirrors is the View Magic. Another with prismatic glasses is the KMQ viewer.[24] A recent usage of this technique is the openKMQ project.[25]

Other display methods without viewers

Autostereoscopy

Autostereoscopic display technologies use optical components in the display, rather than worn by the user, to enable each eye to see a different image. Because headgear is not required, it is also called "glasses-free 3D". The optics split the images directionally into the viewer's eyes, so the display viewing geometry requires limited head positions that will achieve the stereoscopic effect. Automultiscopic displays provide multiple views of the same scene, rather than just two. Each view is visible from a different range of positions in front of the display. This allows the viewer to move left-right in front of the display and see the correct view from any position. The technology includes two broad classes of displays: those that use head-tracking to ensure that each of the viewer's two eyes sees a different image on the screen, and those that display multiple views so that the display does not need to know where the viewers' eyes are directed. Examples of autostereoscopic displays technology include lenticular lens, parallax barrier, volumetric display, holography and light field displays.

Holography

Laser holography, in its original "pure" form of the photographic transmission hologram, is the only technology yet created which can reproduce an object or scene with such complete realism that the reproduction is visually indistinguishable from the original, given the original lighting conditions.[citation needed] It creates a light field identical to that which emanated from the original scene, with parallax about all axes and a very wide viewing angle. The eye differentially focuses objects at different distances and subject detail is preserved down to the microscopic level. The effect is exactly like looking through a window. Unfortunately, this "pure" form requires the subject to be laser-lit and completely motionless—to within a minor fraction of the wavelength of light—during the photographic exposure, and laser light must be used to properly view the results. Most people have never seen a laser-lit transmission hologram. The types of holograms commonly encountered have seriously compromised image quality so that ordinary white light can be used for viewing, and non-holographic intermediate imaging processes are almost always resorted to, as an alternative to using powerful and hazardous pulsed lasers, when living subjects are photographed.

Although the original photographic processes have proven impractical for general use, the combination of computer-generated holograms (CGH) and optoelectronic holographic displays, both under development for many years, has the potential to transform the half-century-old pipe dream of holographic 3D television into a reality; so far, however, the large amount of calculation required to generate just one detailed hologram, and the huge bandwidth required to transmit a stream of them, have confined this technology to the research laboratory.

In 2013, a Silicon valley Company LEIA Inc started manufacturing holographic displays well suited for mobile devices (watches, smartphones or tablets) using a multi-directional backlight and allowing a wide full-parallax angle view to see 3D content without the need of glasses.[26]

Volumetric displays

Volumetric displays use some physical mechanism to display points of light within a volume. Such displays use voxels instead of pixels. Volumetric displays include multiplanar displays, which have multiple display planes stacked up, and rotating panel displays, where a rotating panel sweeps out a volume.

Other technologies have been developed to project light dots in the air above a device. An infrared laser is focused on the destination in space, generating a small bubble of plasma which emits visible light.

Integral imaging

Integral imaging is a technique for producing 3D displays which are both autostereoscopic and multiscopic, meaning that the 3D image is viewed without the use of special glasses and different aspects are seen when it is viewed from positions that differ either horizontally or vertically. This is achieved by using an array of microlenses (akin to a lenticular lens, but an X–Y or "fly's eye" array in which each lenslet typically forms its own image of the scene without assistance from a larger objective lens) or pinholes to capture and display the scene as a 4D light field, producing stereoscopic images that exhibit realistic alterations of parallax and perspective when the viewer moves left, right, up, down, closer, or farther away.

Wiggle stereoscopy

Wiggle stereoscopy is an image display technique achieved by quickly alternating display of left and right sides of a stereogram. Found in animated GIF format on the web. Online examples are visible in the New-York Public Library stereogram collection. The technique is also known as "Piku-Piku".[27]

Stereo photography techniques

For general purpose stereo photography, where the goal is to duplicate natural human vision and give a visual impression as close as possible to actually being there, the correct baseline (distance between where the right and left images are taken) would be the same as the distance between the eyes.[28] When images taken with such a baseline are viewed using a viewing method that duplicates the conditions under which the picture is taken then the result would be an image pretty much the same as what would be seen at the site the photo was taken. This could be described as "ortho stereo."

However, there are situations in which it might be desirable to use a longer or shorter baseline. The factors to consider include the viewing method to be used and the goal in taking the picture. The concept of baseline also applies to other branches of stereography, such as stereo drawings and computer generated stereo images, but it involves the point of view chosen rather than actual physical separation of cameras or lenses.

Stereo window

The concept of the stereo window is always important, since the window is the stereoscopic image of the external boundaries of left and right views constituting the stereoscopic image. If any object, which is cut off by lateral sides of the window, is placed in front of it, an effect results that is unnatural and is undesirable, this is called a "window violation". This can best be understood by returning to the analogy of an actual physical window. Therefore, there is a contradiction between two different depth cues: some elements of the image are hidden by the window, so that the window appears as closer than these elements, and the same elements of the image appear as closer than the window. So that the stereo window must always be adjusted to avoid window violations.

Some objects can be seen in front of the window, as far as they don't reach the lateral sides of the window. But these objects can not be seen as too close, since there is always a limit of the parallax range for comfortable viewing.

If a scene is viewed through a window the entire scene would normally be behind the window, if the scene is distant, it would be some distance behind the window, if it is nearby, it would appear to be just beyond the window. An object smaller than the window itself could even go through the window and appear partially or completely in front of it. The same applies to a part of a larger object that is smaller than the window. The goal of setting the stereo window is to duplicate this effect.

Therefore, the location of the window versus the whole of the image must be adjusted so that most of the image is seen beyond the window. In the case of viewing on a 3D TV set, it is easier to place the window in front of the image, and to let the window in the plane of the screen.

On the contrary, in the case of projection on a much larger screen, it is much better to set the window in front of the screen (it is called "floating window"), for instance so that it is viewed about two meters away by the viewers sit in the first row. Therefore, these people will normally see tha background of the image at the infinite. Of course the viewers seated beyond will see the window more remote, but if the image is made in normal conditions, so that the first row viewers see this background at the infinite, the other viewers, seated behind, will also see this background at the infinite, since the parallax of this background is equal to the average human interocular.

The entire scene, including the window, can be moved backwards or forwards in depth, by horizontally sliding the left and right eye views relative to each other. Moving either or both images away from the center will bring the whole scene away from the viewer, whereas moving either or both images toward the center will move the whole scene toward the viewer. This is possible, for instance, if two projectors are used for this projection.

In stereo photography window adjustments is accomplished by shifting/cropping the images, in other forms of stereoscopy such as drawings and computer generated images the window is built into the design of the images as they are generated.

The images can be cropped creatively to create a stereo window that is not necessarily rectangular or lying on a flat plane perpendicular to the viewer’s line of sight. The edges of the stereo frame can be straight or curved and, when viewed in 3D, can flow toward or away from the viewer and through the scene. These designed stereo frames can help emphasize certain elements in the stereo image or can be an artistic component of the stereo image.

Uses

While stereoscopic images have typically been used for amusement, including stereographic cards, 3D films, stereoscopic video games, printings using anaglyph and pictures, posters and books of autostereograms, there are also other uses of this technology.

Art

Salvador Dalí created some impressive stereograms in his exploration in a variety of optical illusions.[29] Red-and-cyan anaglyph stereoscopic images have also been painted by hand.[30]

Education

In the 19th Century, it was realized that stereoscopic images provided an opportunity for people to experience places and things far away, and many tour sets were produced, and books were published allowing people to learn about geography, science, history, and other subjects.[31] Such uses continued till the mid 20th Century, with the Keystone View Company producing cards into the 1960s.

Space exploration

The Mars Exploration Rovers, launched by NASA in 2003 to explore the surface of Mars, are equipped with unique cameras that allow researchers to view stereoscopic images of the surface of Mars.

The two cameras that make up each rover's Pancam are situated 1.5m above the ground surface, and are separated by 30 cm, with 1 degree of toe-in. This allows the image pairs to be made into scientifically useful stereoscopic images, which can be viewed as stereograms, anaglyphs, or processed into 3D computer images.[32]

The ability to create realistic 3D images from a pair of cameras at roughly human-height gives researchers increased insight as to the nature of the landscapes being viewed. In environments without hazy atmospheres or familiar landmarks, humans rely on stereoscopic clues to judge distance. Single camera viewpoints are therefore more difficult to interpret. Multiple camera stereoscopic systems like the Pancam address this problem with unmanned space exploration.

Clinical uses

Stereogram cards and vectographs are used by optometrists, ophthalmologists, orthoptists and vision therapists in the diagnosis and treatment of binocular vision and accommodative disorders.[33]

Mathematical, scientific and engineering uses

Stereopair photographs provided a way for 3-dimensional (3D) visualisations of aerial photographs; since about 2000, 3D aerial views are mainly based on digital stereo imaging technologies. One issue related to stereo images is the amount of disk space needed to save such files. Indeed, a stereo image usually requires double of the space of a normal image. Recently, computer vision scientists tried to find techniques to attack the visual redundancy of stereopairs with the aim to define compressed version of stereopair files.[34][35] Cartographers generate today stereopairs using computer programs in order to visualise topography in three dimensions.[36] Computerised stereo visualisation applies stereo matching programs.[37] In biology and chemistry, complex molecular structures are often rendered in stereopairs. The same technique can also be applied to any mathematical (or scientific, or engineering) parameter that is a function of two variables, although in these cases it is more common for a three-dimensional effect to be created using a 'distorted' mesh or shading (as if from a distant light source).

Bibliography

Footnotes

  1. ^ "The Kaiser (Emperor) Panorama". June 9, 2012. 
  2. ^ στερεός Tufts.edu, Henry George Liddell, Robert Scott, A Greek-English Lexicon, on Perseus Digital Library
  3. ^ σκοπέω, Henry George Liddell, Robert Scott, A Greek-English Lexicon, on Perseus Digital Library
  4. ^ Exercises in Three Dimensions: About 3D, Tom Lincoln, 2011
  5. ^ Flight Simulation, J. M. Rolfe and K. J. Staples, Cambridge University Press, 1986, page 134
  6. ^ Exercises in Three Dimensions, Tom Lincoln, 2011
  7. ^ a b Contributions to the Physiology of Vision.—Part the First. On some remarkable, and hitherto unobserved, Phenomena of Binocular Vision. By CHARLES WHEATSTONE, F.R.S., Professor of Experimental Philosophy in King's College, London. Stereoscopy.com
  8. ^ Welling, William. Photography in America, page 23
  9. ^ International Stereoscopic Union, 2006, "Stereoscopy", Numbers 65-72, p.18
  10. ^ Stereo Realist Manual, p. 375.
  11. ^ Stereo Realist Manual, pp. 377–379.
  12. ^ Fay Huang, Reinhard Klette, and Karsten Scheibe: Panoramic Imaging (Sensor-Line Cameras and Laser Range-Finders). Wiley & Sons, Chichester, 2008
  13. ^ Dornaika, F.; Hammoudi, K (2009). "Extracting 3D Polyhedral Building Models from Aerial Images using a Featureless and Direct Approach" (PDF). Proc. IAPR/MVA. Retrieved 2010-09-26. 
  14. ^ "Eyecare Trust". Eyecare Trust. Retrieved 29 March 2012. 
  15. ^ "Daily Telegraph Newspaper". The Daily Telegraph. Retrieved 29 March 2012. 
  16. ^ "Understanding Requirements for High-Quality 3D Video: A Test in Stereo Perception". 3droundabout.com. 19 December 2011. Retrieved 29 March 2012. 
  17. ^ The Logical Approach to Seeing 3D Pictures. www.vision3d.com by Optometrists Network. Retrieved 2009-08-21
  18. ^ How To Freeview Stereo (3D) Images. Greg Erker. Retrieved 2009-08-21
  19. ^ How to View Photos on This Site. Stereo Photography – The World in 3D. Retrieved 2009-08-21
  20. ^ Tseng, Belle; Anastassiou, Dimitris. "Compatible Video Coding of Stereoscopic Sequences using MPEG-2's Scalability and Interlaced Structure" (PDF). Columbia University. Retrieved 8 July 2014. 
  21. ^ "Seeing is believing""; Cinema Technology, Vol 24, No.1 March 2011
  22. ^ http://www.dpvotheatrical.com/
  23. ^ Exercises in Three Dimensions: About 3D
  24. ^ "Glossary". June 8, 2012. 
  25. ^ "openKMQ". June 8, 2012. 
  26. ^ "A Multi-Directional Backlight For A Wide-Angle, Glasses-Free 3D Display", Nature, 2013
  27. ^ http://www.shortcourses.com/stereo/stereo1-17.html
  28. ^ DrT (2008-02-25). "Dr. T". Drt3d.blogspot.com. Retrieved 2012-03-04. 
  29. ^ Horibuchi, S. (1994). Salvador Dalí: the stereo pair artist. In Horibuchi, S. (Ed.), Stereogram (pp.9, pp.42). San Francisco: Cadence Books. ISBN 0-929279-85-9
  30. ^ Exercises in Three Dimensions, Tom Lincoln, 2011
  31. ^ University of Virginia The Stereoscope In America, accessed 21 March 2009.
  32. ^ "Pancam technical brief" (PDF). Cornell University. Retrieved 2006-06-30. 
  33. ^ Bartiss, OD MD, Michael (2005-01-25). "Convergence Insufficiency". WebMD. Retrieved 2006-06-30. 
  34. ^ Algorithm for stereoscopic image compression.
  35. ^ Ortis, A., Rundo, F., Di Giore, G., & Battiato, S. (2013, September). Adaptive compression of stereoscopic images. In International Conference on Image Analysis and Processing (pp. 391-399). Springer Berlin Heidelberg.
  36. ^ David F. Watson (1992). Contouring. A Guide to the Analysis and Display of Spatial Data (with programs on diskette). In: Daniel F. Merriam (Ed.); Computer Methods in the Geosciences; Pergamon / Elsevier Science, Amsterdam; 321 pp. ISBN 0-08-040286-0
  37. ^ Reinhard Klette (2014). "Concise Computer Vision" (see Chapter 8 for stereo matching). Springer, London; 429 pp. ISBN 978-1-4471-6319-0

Sources

  • Simmons, Gordon (March–April 1996). "Clarence G. Henning: The Man Behind the Macro". Stereo World. 23 (1): 37–43. 
  • Willke, Mark A.; Zakowski, Ron (March–April 1996). "A Close Look into the Realist Macro Stereo System". Stereo World. 23 (1): 14–35. 
  • Morgan, Willard D.; Lester, Henry M. (October 1954). Stereo Realist Manual. and 14 contributors. New York: Morgan & Lester. OCLC 789470. 

Further reading

  • Scott B. Steinman, Barbara A. Steinman and Ralph Philip Garzia. (2000). Foundations of Binocular Vision: A Clinical perspective. McGraw-Hill Medical. ISBN 0-8385-2670-5

Archival Collections

Other



This article uses material from the Wikipedia article "Stereoscopy", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

CAD CAM (Mechanical) Dictionary

3D,Models,Catalogs,Drawings,Library,Symbols,Objects,OEM