Licensed under Creative Commons Attribution-Share Alike 2.0 (Original: lyzadanger
Derivative work: Diliff).
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (May 2015) (Learn how and when to remove this template message) |
The Food Industry is a complex, global collective of diverse businesses that supplies most of the food consumed by the world population. Only subsistence farmers, those who survive on what they grow, and hunter-gatherers can be considered outside of the scope of the modern food industry.
The food Industry includes:
It is challenging to find an inclusive way to cover all aspects of food production and sale. The Food Standards Agency describes it thus:
The Economic Research Service of the USDA uses the term food system to describe the same thing:
Agriculture is the process of producing food, feeding products, fiber and other desired products by the cultivation of certain plants and the raising of domesticated animals (livestock). The practice of agriculture is also known as "farming". Scientists, inventors, and others devoted to improving farming methods and implements are also said to be engaged in agriculture. 1 in 3 people worldwide are employed in agriculture,[4] yet it only contributes 3% to global GDP.[5]
Agronomy is the science and technology of producing and using plants for food, fuel, fibre, and land reclamation. Agronomy encompasses work in the areas of plant genetics, plant physiology, meteorology, and soil science. Agronomy is the application of a combination of sciences. Agronomists today are involved with many issues including producing food, creating healthier food, managing environmental impact of agriculture, and extracting energy from plants.[6]
Food processing includes the methods and techniques used to transform raw ingredients into food for human consumption. Food processing takes clean, harvested or slaughtered and butchered components and uses them to produce marketable food products. There are several different ways in which food can be produced.
One off production: This method is used when customers make an order for something to be made to their own specifications, for example a wedding cake. The making of one-off products could take days depending on how intricate the design is.
Batch production: This method is used when the size of the market for a product is not clear, and where there is a range within a product line. A certain number of the same goods will be produced to make up a batch or run, for example a bakery may bake a limited number of cupcakes. This method involves estimating consumer demand.
Mass production: This method is used when there is a mass market for a large number of identical products, for example chocolate bars, ready meals and canned food. The product passes from one stage of production to another along a production line.
Just-in-time (JIT) (production): This method of production is mainly used in restaurants. All components of the product are available in-house and the customer chooses what they want in the product. It is then prepared in a kitchen, or in front of the buyer as in sandwich delicatessens, pizzerias, and sushi bars.
The food industry has a large influence on consumerism. Organizations, such as The American Academy of Family Physicians (AAFP), have been criticized for accepting monetary donations from companies within the food industry, such as Coca-Cola.[7] These donations have been criticized for creating a conflict of interest and favoring an interest such as financial gains.[7]
Since World War II, agriculture in the United States and the entire national food system in its entirety has been characterized by models that focus on monetary profitability at the expense of social and environmental integrity.[8] Regulations exist to protect consumers and somewhat balance this economic orientation with public interests for food quality, food security, food safety, animal well-being, environmental protection and health.[9]
A vast global cargo network connects the numerous parts of the industry. These include suppliers, manufacturers, warehousers, retailers and the end consumers. Wholesale markets for fresh food products have tended to decline in importance in urbanizing countries, including Latin America and some Asian countries as a result of the growth of supermarkets, which procure directly from farmers or through preferred suppliers, rather than going through markets.
The constant and uninterrupted flow of product from distribution centers to store locations is a critical link in food industry operations. Distribution centers run more efficiently, throughput can be increased, costs can be lowered, and manpower better utilized if the proper steps are taken when setting up a material handling system in a warehouse.[10]
With worldwide urbanization,[11] food buying is increasingly removed from food production. During the 20th century, the supermarket became the defining retail element of the food industry. There, tens of thousands of products are gathered in one location, in continuous, year-round supply.
Food preparation is another area where the change in recent decades has been dramatic. Today, two food industry sectors are in apparent competition for the retail food dollar. The grocery industry sells fresh and largely raw products for consumers to use as ingredients in home cooking. The food service industry by contrast offers prepared food, either as finished products, or as partially prepared components for final "assembly". Restaurants, cafes, bakeries and mobile food trucks provide opportunities for consumers to purchase food.
Modern food production is defined by sophisticated technologies. These include many areas. Agricultural machinery, originally led by the tractor, has practically eliminated human labor in many areas of production. Biotechnology is driving much change, in areas as diverse as agrochemicals, plant breeding and food processing. Many other types of technology are also involved, to the point where it is hard to find an area that does not have a direct impact on the food industry. As in other fields, computer technology is also a central force, with computer networks and specialized software providing the support infrastructure to allow global movement of the myriad components involved.
As consumers grow increasingly removed from food production, the role of product creation, advertising, and publicity become the primary vehicles for information about food. With processed food as the dominant category, marketers have almost infinite possibilities in product creation. Of the food advertised to children on television 73% is fast or convenience foods.[12]
Until the last 100 years, agriculture was labor intensive. Farming was a common occupation and millions of people were involved in food production. Farmers, largely trained from generation to generation, carried on the family business. That situation has changed dramatically today. In America in 1870, 70-80 percent of the US population was employed in agriculture.[13] As of 2008[update], less than 2 percent of the population is directly employed in agriculture.,[14][15] and about 80% of the population lives in cities. The food industry as a complex whole requires an incredibly wide range of skills. Several hundred occupation types exist within the food industry.
Work in the food industry traditionally involves gendered divisions of labor. Perceived and actual physical strength, and the ability to use technology[16] define the boundaries between the work of men and women. According to a 2012 survey[17] by the US Bureau of Labor Statistics, men earn median weekly wages of $433 as compared to $389 earned by women in the same food preparation and service jobs. Women are also less likely to have low income mobility, as they make up less than 33% of paid cooks and less than 18% of head chefs in restaurants,[16] but over 65% of the lowest skilled food preparers and servers.[17] Men are found to be employed in ownership, managerial, and supervisory positions, while women often work in subordinate, clerical positions.[18]
Occupational sex segregation in the food industry is maintained by gendered norms and interactions. Women are faced with the challenge of being assertive and professionally competent while also demonstrating gender normative, traditionally feminine passivity.[19] They are more likely to be subject to sexual abuse and violence in the workplace.[20] Obstacles more likely to be faced by women—such as pay inequality, lack of role models and mentoring, discrimination and harassment, and family needs—prevent career advancement.[21]
This article uses material from the Wikipedia article "Food industry", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D - 3D CAD - 3D Models - 3D Library - Mechanical Engineering - Maschinenbau , Architecture Engineering - Architektur - BIM, Electrical Engineering - Elektrotechnik, Mechatronic - Mechatronik, Plant Design - Anlagenbau, Marine - Offshore Onshore - Food Service - Interior Architecture Innenarchitektur - Furnitures Möbel - Automotive - IoT Internet Of Things Industry 4.0 Industrie 4.0 Digital Twin Manufacturing 2025 - Chemistry - Food Service - Landscape Architecture - Exterior Architecture