A drum kit — also called a drum set, trap set, or simply drums — is a collection of drums and other percussion instruments, typically cymbals, which are set up on stands to be played by a single player, with drumsticks held in both hands, and the feet operating pedals that control the hi-hat cymbal and the beater for the bass drum. A drum kit consists of a mix of drums (categorized classically as membranophones, Hornbostel-Sachs high-level classification 2) and idiophones - most significantly cymbals, but can also include the woodblock and cowbell (classified as Hornbostel-Sachs high-level classification 1). In the 2000s, some kits also include electronic instruments (Hornbostel-Sachs classification 53). Also, both hybrid (mixing acoustic instruments and electronic drums) and entirely electronic kits are used.
A standard modern kit (for a right-handed player), as used in popular music and taught in music schools, contains:
A snare drum, mounted on a stand, placed between the player's knees and played with drum sticks (which may include rutes or brushes)
A bass drum, played by a pedal operated by the right foot, which moves a felt-covered beater
One or more toms, played with sticks or brushes (usually three toms: rack tom 1 and 2, and floor tom)
A hi-hat (two cymbals mounted on a stand), played with the sticks, opened and closed with left foot pedal (it can also produce sound with the foot alone)
One or more cymbals, mounted on stands, played with the sticks
All of these are classed as non-pitched percussion, allowing for the music to be scored using percussion notation, for which a loose semi-standardized form exists for the drum kit. If some or all of them are replaced by electronic drums, the scoring and most often positioning remains the same, allowing a standard teaching approach. The drum kit is usually played while seated on a drum stool or throne. The drum kit differs from instruments that can be used to produce pitched melodies or chords, even though drums are often placed musically alongside others that do, such as the guitar or piano. The drum kit is a part of the standard rhythm section used in many types of popular and traditional music styles, ranging from rock and pop to blues and jazz. Other standard instruments used in the rhythm section include the piano, electric guitar, electric bass, and keyboards.
Many drummers extend their kits from this basic pattern, adding more drums, more cymbals, and many other instruments including pitched percussion. In some styles of music particular extensions are normal, for example double bass drums in heavy metal music and the enlarged kits used by some progressive drummers, which may include unusual instruments such as gongs. Some performers, such as some rockabilly drummers, use small kits that omit elements from the basic setup. Some drum kit players may have other roles in the band, such as providing backup vocals, or less commonly, lead vocals.