Mercedes-AMG GmbH, commonly known as AMG, is the high performance division of Mercedes-Benz. AMG independently hires engineers, manufactures and customizes Mercedes-Benz AMG vehicles. Mercedes-AMG is headquartered in Affalterbach, Baden-Württemberg, Germany. AMG was originally an independent engineering firm specializing in performance improvements for Mercedes-Benz vehicles; Daimler-Benz AG took a controlling interest in 1999, then became sole owner of AMG in 2005. Mercedes-AMG GmbH is now a wholly owned subsidiary of Daimler AG.
AMG models typically have more aggressive looks, a higher level of performance, better handling, better stability and more extensive use of carbon fibre than their regular Mercedes-Benz counterparts. AMG models are typically the most expensive and highest-performing variant of each Mercedes-Benz class.
AMG variants are usually badged with two numerals, as opposed to regular Mercedes-Benz vehicles, which have three (e.g., C 63 as opposed to C 350). Traditionally, the two numerical digits signified the engine's displacement size, however, recent models have deviated from such correlation.