powered by CADENAS

FAQ Options

FAQ Information

FAQ Categories

Categories:

FAQ Description

How to add Augmented Reality (AR) in PARTcloud.net and 3D CAD models with various environments

Augmented Reality (AR) is understood as computer-assisted extension of the perception of reality. Frequently, images or videos are supplemented with additional information or virtual objects by means of overlaying or superimposing.

 

 

1.Users have to login at PARTcloud.net or create an account. If you are already registered for the 3D CAD models download portal PARTcommunity, this is also valid for PARTcloud.net.The components are uploaded and the information as well as details filled in, so that the 3D CAD model can be found more easily by other users.

 

 

 

2.After uploading, the 3D CAD model appears in your own portfolio.

 

3. The users now activate the environment function by moving the cursor to the lower bar and clicking the last button.

 

4. A new window appears, where the environments can be selected. Here are different environments available to the users, such as city silhouette and floor variants such as parquet. Both options can be selected at the same time.

 

5. At the end, the users obtain their 3D model with the selected background. Now they can put the model in the scene accordingly per screenshot or in the PARTcloud.net app or add the image at social networks.

 

 

 

 

 

 

100% users marked this FAQ as helpful.
|
Was this answer helpful?
1 vote