powered by CADENAS



Social Share

News Entry

(EN) So Autodesk Fusion 360 users can now do their design work even faster

  • New user interface of the integrated “parts4cad” app from CADENAS simplifies designs

    Since the beginning of 2016, users have benefitted from the cloud-based design and planning software Autodesk® Fusion 360™ with the fully-integrated CADENAS app “parts4cad” and its millions of 3D models from over 400 certified manufacturer catalogs. A new version of the cloud-based CAD solution for 3D modelling has been available since the end of 2016. Thus, a completely new user interface of the 3D CAD models download service “parts4cad” from CADENAS was introduced.

    The desired components can be individually configured more easily and quickly, thanks to the new “parts4cad” user interface and then directly integrated into the existing design in Autodesk Fusion 360.

    Simple integration of a 3D CAD model by “parts4cads” directly into Autodesk Fusion 360

    "Insert a manufacturer part" can be found in the tab "Insert". This leads the user directly to “parts4cad”.

    parts4cad in Autodesk Fusion 360

    In “parts4cad”, the user can then retrieve the desired manufacturer catalog.

    parts4cad in Autodesk Fusion 360

    The selected component can now be individually configured and integrated into Autodesk Fusion 360.

    parts4cad in Autodesk Fusion 360

    The 3D CAD model can be integrated into an existing design in Autodesk Fusion 360.

    parts4cad in Autodesk Fusion 360

    Cloud-based design not dependent on location and time

    Autodesk Fusion 360 is a comprehensive cloud-based solution for 3D modelling and the first 3D CAD/CAM tool of its kind to span over the entire product development process in a cloud-based tool. Designers and engineers create their product designs in the cloud in 3D and work internationally together with other participants. The cloud technology behind Autodesk Fusion 360 makes it possible that the user has access at any time, regardless of location and with any mobile end device or Internet browser.

    More information on “parts4cad” in Autodesk Fusion 360 you can find here.


1 comment