Tata Steel and CADENAS are working closely together to meet the requirements of the BIM industry perfectly. In 2018 Tata Steel launched their pioneering, BIM Tool the "DNA Profiler" granting engineers and architects easy access to configurable products and instant BIM CAD data, directly from Tata Steel’s website. Now Alex Small, BIM & digital platforms manager at Tata Steel, gives insights into current developments and trends in the BIM sector:
Over the past few years a wide selection of online, third party, BIM hosting companies have provided their platforms for professionals at the design stage of the construction process with data rich 3D objects. Many specifiers understand the need to embrace this new digitalisation of the construction sector thus creating demand. Potentially some market sectors have considered making BIM information a necessity during the design stage in the near future, for example, public sector projects within the UK. Alex Small, BIM & digital platforms manager at Tata Steel, explains more.
Many organisations have an array of product ranges, types and sizes that are all supported by 3D CAD files. These can be provided in a series of formats such as Revit, ArchiCAD and Tekla to name but a few. Here at Tata Steel we provide over 6,100 unique products with new products being added to the range regularly and existing products being updated and revolutionised on a constant basis – can this be easily managed across third party BIM providers?
With over 17,500 micro construction manufacturers in the UK alone is it feasible to think that the cost and resource to manage and update a library of data files across an array of platforms is realistic? With this in mind, Architects are utilising unmaintained BIM information during the design stage, upon realising this many are reverting back to manufacturers directly to obtain the most recent ‘live’ objects. This could be seen as a step backwards in terms of digitalisation within the constructions sector and losing the trust of designers in the long term.
In October 2018, the UK BIM Alliance published it’s ‘A Fresh Way Forward for Product Data’ following stakeholder engagement from within the industry. Some of the key outcomes included the importance of product data being highly relevant, accurate, version controllable and useable. In order to achieve these goals it was decided that the below must be considered going forward:
By meeting the above criteria manufacturers will have control over their product range, data and information in one ‘single hub’ and give them confidence that any third party BIM hosts will have the same, accurate data. This will provide Architects and Specifiers with a much more reliable source of product data and help grow their confidence in utilising these much needed digitisation methods.
Working with IBM and CADENAS Tata Steel have already taken the necessary steps to meet with the above requirements.
Key benefits of Tata Steel’s DNA Profiler:
The above provides Architects, Contractors and Engineers with ‘live’ data and BIM information.
Tata Steel are also developing a plug-in for all CAD software programmes that will link directly to Tata Steel’s live object database – this will link and push current, up to date data directly from Tata Steel’s database into related products utilised within specifiers design(s) further ensuring live data is provided.
The success of full digitalisation within the construction industry relies heavily upon the requirement of open data standards, interconnected databases and systems. This ensures the accuracy and reliability of the provided data to the market. Tata Steel has developed an API, a set of functions and procedures that allow the creation of applications such as BIM hosting websites with direct access to the data of Tata Steel’s product database.
This is a challenging and exciting time for the industry with Tata Steel looking to lead the way in assisting and improving the industry via data-driven tools and platforms and sharing our processes to help make digitalisation a reality. Having the right partners, such as IBM, is key to this success and a bright, connected and enabled future awaits us all.
To access BIM information for over 6,000 Tata Steel construction products visit www.tatasteeldnaprofiler.com/register
The original Tata Steel news can be found at: www.tatasteelconstruction.com/en_GB/About-us/news/BIM-Product-Data
Comments