Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Note | |
---|---|
Concerning tolerances, please ensure appropriate config settings! With very small parts (<0,01mm) and very large parts with small details (40m steel band with 1mm roundings), problems may occur. |
As of V11SP4 there
are three default templates für the Q&S Import ($CADENAS_SETUP/partsol.cfg
):
These templates should be used in this sequence.
Options0=OPTPAGEPARASOLIDCOMMON=ParameterTemplate=string=Template_QAS_strict ;Options0=OPTPAGEPARASOLIDCOMMON=ParameterTemplate=string=Template_QAS_lazy ;Options0=OPTPAGEPARASOLIDCOMMON=ParameterTemplate=string=Template_QAS_lazy_crash
If the part to be
imported contains 2D faces, which however should not be imported, $CADENAS_SETUP/ifparasolid.cfg
has to be
adjusted.
- ImportProcessorPreFilterBody on 5601 or set
- ImportProcessorPostFilterBody on 5601.
For ImportProcessorPostFilterBody: Copy line from ImportProcessorPreFilterBody, adjust it and set on 5601.
Difference: With ImportProcessorPreFilterBody 2D faces won't appear at all when importing, with ImportProcessorPostFilterBody the elements are removed.