Mark the
required project and click on the context menu command Save as CIP.
-> The
dialog box Create CIP file is opened.
Settings:
CIP file to create: Apply the path
in which the *.cip file will be temporarily stored.
Part directory: The path of origin
of the project is entered per default. If you do not change it,
the *.cip file is then placed into this path when
starting.
Note
When opening the *.cip file, the PARTdataManager is
automatically started. The cipped part is imported into the directory
tree and the index is automatically created.
In PARTproject the cipped file
is only visible after restarting the program.